Hello Sir,
We have DM368 based custom board. We are facing problem of deinterlacing in video recording. According to our understanding two methods are available to resolve the deinterlacing problem.
1. By using interlaced encoding.
We followed the following links to set the Input video types as Interlaced in H.264 encoder configuration. At this link, output storage mechanism was not described. So we would like to know, how output video stored in memory?
processors.wiki.ti.com/.../DM36x_Interlace_Encoding_FAQs
2. Another solution is by using deinterlacing algorithm. For DM368, DVSDK 04_02_00_06 is the latest release of DVSDK. In this DVSDK, deinterlacing algorithm support is not available. We gone through the forums and found that TI provides hardware accelerated based De-Interlacing algorithms with DVSDK. We download the latest release(04_03_00_06) of dvsdk for DM3730 because for DM368 it is not available. In DVSDK 4_03_00_06 Deinterlacer support is available for OMAP3530. We would like to know is it feasible to use the provided deinterlacing algorihtm with DM368? If yes, then how we can use this deinterlacing algorithm for DM368?
Thanks & Regards
Uma Shanker