Hi,
I have a main code on a main.c file and a couple tasks in the TI RTOS cfg file. Everything compiles and works fine.
But, when I include a class declaration and some other functions in a crypto.cpp and crypto.h files that I have written there are a few compiling problems.
1) Even though I included in main.c the crypto.h, it says class was undefined. After looking around on the forum I solved this changing my main.c file to main.cpp. Another option that solves this is keep main.c file and mark the compiler advanced option for treating c files as cpp files.
2) The problem now is that I am getting a unresolved symbol error for the tasks I am using.
CCS has an example with a cpp file called bigtime for TM4C129. This example doesn't have tasks and compiles just fine. But when I include a task on it, it shows the same unresolved symbol error I got before.
Can anyone please help me to solve this issue?
Thank you,
Paulo