This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Video corruption when running Windows CE Media Player on OMAP3530

Other Parts Discussed in Thread: OMAP3530

I am using a Torpedo SOM with OMAP3530 to drive an XGA (1024x768) LCD panel. Software version is WinCE 6.0 BSP1.1.2 provided by LogicPD. All static graphics and display are okay. The problems occur when I open a video file of smaller size with Windows Media Player, streak lines will run across the screen. If I move the display window partially outside of the LCD display, the view port would lose sync while the rest of the desktop would still be fine. If I resize the Media Player view port smaller, the whole screen would become corrupted.

Are there any adjustments I need to do to the software drivers in order to run video on by LCD panel? The CE image was rebuilt using Visual Studio 2005. Thanks.

BYeung