This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM35xx USB registers and its base address

Hello every one!

I did try to search the Base address of the registers, which are listed in the Table 20-9 of the TRM (Jun 2010). And found only one place with it in the Table 2-3.

But.

In the Table 20-9 the address space is about 27kB, because the last offset in that table is 0x6800 - 16xN + 8

And in the table 2-3 the length of the USB device is only 4 K bytes  from 0x480AB000 till 0x480ABFFF.

And if I add  0x6800 to that base address 0x480AB000 , then I would try to access the reserver area. And what is most weired, is that the registers in a middle of the table 20-9 would be places in the address spaces of other devices.

So the question is - where can i find the REAL base address of the registers, which are described in the Table 20-9 "Universal Serial Bus (USB) Registers".

And what address is it?

 

Thank You in advance,

Alexey