Other Parts Discussed in Thread: AM1808, OMAP-L138
Hello
I encountered a problem of flashing system images into nand of am1808 evm (Zoom AM1808 EVM Development Kit) under CCS v4 evironment.
I followed up all procedures described here: set up target configuration, build project files, connect target, and run nand writer.
Only a message showed on the console: Starting OMAP-L138 NANDWriter, then hang there.
But, no ask for input arm-nand-ais.bin and u-boot.bin to burn both images into nand flash.
All demo programs in the
package AM1808
BSL-1.0-Setup run well on the board, so it seems not to be a hardware issue.
So, could you kindly tell me how to solve this issue?
And, can other utility like sfh_OMAP-L138 do the same thing?
Thanks a lot for help.