Hello,
I have problem to bring up an AM3352 processor.
If I start the prozessor I can see on UART0 eight times an "C". Sometime I get continuous "C"´s with a time distance of 300ms. Or I get some "wrong" characters on UART0.
My sysboot pins are:
MSB LSB
1000 0000 0100 0111
-> 25MHz
-> RMII
-> Bootsequence EMAC1 MMC0 XIP NAND
Why I get sometimes continuous C sequences or sometimes only eight?
There is possible a problem on clock because I get sometime sequences with broken characters on UART0?