Other Parts Discussed in Thread: SYSBIOS, OMAPL138
Hey,
it seems to be expected that static variables aren't initialized in COFF mode, but all the sources seem to assume that it is different by default for the EABI compiler. Yet I'm still experiencing the problem with the current compiler set to EABI.
I'm running CCS6.2 with XDCtools 3.25.3.72 and sys/bios 6.35.6.56, targeting OMAP L138.
There is custom linker script added to the project in addition to the generated ones. The variables not being initialized do NOT belong to the custom defined sections:
SECTIONS
{
// !!! IMPORTANT: IROM is not programmable on OMAP-L138 !!!
// ------------- ACQ hwi stuff into L2 ------------------------
.text_fast: { *.*(.text.fast*) } > IRAM
.data_fast: { *.*(.data.fast*) } > IRAM
.data_quick: { *.*(.data.quick*) } > L3_CBA_RAM
// ------------- Kernel stuff into fast memory -----------------
/* place all the knl APIs in IRAM */
.knl: { *.*(.text:*ti_sysbios_knl*) } > IRAM
/* place all the Hwi APIs in IROM */
.hwi: { *.*(.text:*ti_sysbios*_Hwi_*) } > IRAM
/* place the remainder of the SYS/BIOS APIs in DDR */
.sysbios: { *.*(.text:*ti_sysbios*) } > DDR
}
The linker script generated by XDCtools under Debug/configPkg looks as follows (I've removed the commented out stuff to reduce size):
-l"/home/maverick/ccsworkspace/_SCARY_PROJECT_NAME_/Debug/configPkg/package/cfg/sysbios_pe674.oe674"
-l"/home/maverick/ti/syslink_2_21_03_11/packages/ti/syslink/ipc/rtos/lib/debug/ti.syslink.ipc.rtos.ae674"
-l"/home/maverick/ccsworkspace/_SCARY_PROJECT_NAME_/src/ipc/ipc.ae674"
-l"/home/maverick/ccsworkspace/_SCARY_PROJECT_NAME_/src/sysbios/sysbios.ae674"
-l"/home/maverick/ti/syslink_2_21_03_11/packages/ti/syslink/utils/rtos/bios6/lib/debug/ti.syslink.utils.rtos.bios6.ae674"
-l"/home/maverick/ti/edma3_lld_02_12_00_20/packages/ti/sdo/edma3/drv/lib/674/debug/edma3_lld_drv.ae674"
-l"/home/maverick/ti/edma3_lld_02_12_00_20/packages/ti/sdo/edma3/rm/lib/omapl138-evm/674/debug/edma3_lld_rm.ae674"
-l"/home/maverick/ti/xdctools_3_25_03_72/packages/ti/targets/rts6000/lib/ti.targets.rts6000.ae674"
-l"/home/maverick/ti/xdctools_3_25_03_72/packages/ti/targets/rts6000/lib/boot.ae674"
--retain="*(xdc.meta)"
--args 0x64
-heap 0x0
-stack 0x1000
MEMORY
{
IROM (RX) : org = 0x11700000, len = 0x100000
IRAM (RWX) : org = 0x11800000, len = 0x20000
L3_CBA_RAM (RWX) : org = 0x80000000, len = 0x20000
DDR (RWX) : org = 0xc6800000, len = 0x1800000
DDR_SHARED (RWX) : org = 0xc6000000, len = 0x800000
}
SECTIONS
{
ti.sdo.ipc.SharedRegion_0: { . += 0x800000;} run > 0xc6000000, type = NOLOAD
ti_sdo_ipc_init: load > DDR, type = NOINIT
}
/*
* Set entry point to the HWI reset vector 0 to automatically satisfy
* any alignment constraints for the boot vector.
*/
-eti_sysbios_family_c64p_Hwi0
/*
* We just modified the entry point, so suppress the "entry point symbol other
* than _c_int00 specified" warning.
*/
--diag_suppress=10063
/* Add the flags needed for SysLink ELF build. */
--dynamic
--retain=_Ipc_ResetVector
/*
* Added symbol to ensure SysBios code is retained when entrypoint is
* something other than _c_int00. This workaround will be removed once
* fixed in the SysBios package
*/
-u _c_int00
/*
* symbolic aliases for static instance objects
*/
xdc_runtime_Startup__EXECFXN__C = 1;
xdc_runtime_Startup__RESETFXN__C = 1;
TSK_idle = ti_sysbios_knl_Task_Object__table__V + 228;
SECTIONS
{
.text: load >> DDR
.ti.decompress: load > DDR
.stack: load > L3_CBA_RAM
GROUP: load > DDR
{
.bss:
.neardata:
.rodata:
}
.cinit: load > DDR
.pinit: load >> DDR
.init_array: load > DDR
.const: load >> DDR
.data: load >> DDR
.fardata: load >> DDR
.switch: load >> DDR
.sysmem: load > DDR
.far: load >> DDR
.args: load > DDR align = 0x4, fill = 0 {_argsize = 0x64; }
.cio: load >> DDR
.ti.handler_table: load > DDR
.c6xabi.exidx: load > DDR
.c6xabi.extab: load >> DDR
.heap: load > DDR
.vecs: load > DDR
.plt: load > DDR
xdc.meta: load > DDR, type = COPY
}
It seems to be an option to add "fill" attribute to the .bss and other sections via sysbios.cfg, but considering the TI documentation says I shouldn't have to change anything for the EABI compiler - I'm confused. The compiler and linker settings seem to be normal:
Compiler flags:
-mv6740 --abi=eabi -Ooff --include_path="/home/maverick/ti/ti-cgt-c6000_8.1.2/include" -g --c99 --define=omapl138 --diag_warning=225 --display_error_number --diag_wrap=off
Linker flags:
-mv6740 --abi=eabi -Ooff -g --c99 --define=omapl138 --diag_warning=225 --display_error_number --diag_wrap=off -z -m"_SCARY_PROJECT_NAME_.map" --heap_size=0x300000 --stack_size=0x1000 -i"/home/maverick/ti/ti-cgt-c6000_8.1.2/lib" -i"/home/maverick/ti/ti-cgt-c6000_8.1.2/include" --reread_libs --define=DSP_CORE=1 --diag_wrap=off --warn_sections --display_error_number --xml_link_info="_SCARY_PROJECT_NAME_linkInfo.xml" --rom_model --zero_init=on
Thank you in advance,
Mav