Other Parts Discussed in Thread: MSP430F5659, SYSBIOS, MSP430DRIVERLIB, MSP430F5529, MSP430F6459, MSP430F5527
I'm not sure if this question is for the compiler or the TI-RTOS forum, but here goes.
After enabling the UIA logger in my application *.cfg file, I get some driver functions overflow (see below).
How do I mitigate this?
I've also included my linker script.
"MSP430F5xx_6xx/ucs.c", line 176: warning #17003-D: relocation from function "privateUCSSourceClockFromDCO" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12ba is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000056, section = ".text:privateUCSSourceClockFromDCO")
"MSP430F5xx_6xx/ucs.c", line 176: warning #17003-D: relocation from function "privateUCSSourceClockFromDCO" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12bc is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x0000005a, section = ".text:privateUCSSourceClockFromDCO")
"MSP430F5xx_6xx/ucs.c", line 140: warning #17003-D: relocation from function "privateUCSSourceClockFromDCO" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b6 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000074, section = ".text:privateUCSSourceClockFromDCO")
"MSP430F5xx_6xx/ucs.c", line 140: warning #17003-D: relocation from function "privateUCSSourceClockFromDCO" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b8 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000078, section = ".text:privateUCSSourceClockFromDCO")
"MSP430F5xx_6xx/ucs.c", line 269: warning #17003-D: relocation from function "privateUCSComputeCLKFrequency" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12ba is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000034, section = ".text:privateUCSComputeCLKFrequency")
"MSP430F5xx_6xx/ucs.c", line 269: warning #17003-D: relocation from function "privateUCSComputeCLKFrequency" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12bc is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000038, section = ".text:privateUCSComputeCLKFrequency")
"MSP430F5xx_6xx/ucs.c", line 227: warning #17003-D: relocation from function "privateUCSComputeCLKFrequency" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b6 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000060, section = ".text:privateUCSComputeCLKFrequency")
"MSP430F5xx_6xx/ucs.c", line 227: warning #17003-D: relocation from function "privateUCSComputeCLKFrequency" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b8 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000064, section = ".text:privateUCSComputeCLKFrequency")
"MSP430F5xx_6xx/ucs.c", line 298: warning #17003-D: relocation from function "UCS_setExternalClockSource" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b6 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000002, section = ".text:UCS_setExternalClockSource")
"MSP430F5xx_6xx/ucs.c", line 298: warning #17003-D: relocation from function "UCS_setExternalClockSource" to symbol "privateXT1ClockFrequency" overflowed; the 20-bit relocated address 0xf12b8 is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x00000006, section = ".text:UCS_setExternalClockSource")
"MSP430F5xx_6xx/ucs.c", line 299: warning #17003-D: relocation from function "UCS_setExternalClockSource" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12ba is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x0000000a, section = ".text:UCS_setExternalClockSource")
"MSP430F5xx_6xx/ucs.c", line 299: warning #17003-D: relocation from function "UCS_setExternalClockSource" to symbol "privateXT2ClockFrequency" overflowed; the 20-bit relocated address 0xf12bc is too large to encode in the 16-bit field (type = 'R_MSP430X_ABS16' (15), file = "C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx/ccs/MSP430F5659.lib<ucs.obj>", offset = 0x0000000e, section = ".text:UCS_setExternalClockSource")
warning #10015-D: output file "scorli-fw.out" cannot be loaded and run on a target system
/* ============================================================================ */
/* Copyright (c) 2016, Texas Instruments Incorporated */
/* All rights reserved. */
/* */
/* Redistribution and use in source and binary forms, with or without */
/* modification, are permitted provided that the following conditions */
/* are met: */
/* */
/* * Redistributions of source code must retain the above copyright */
/* notice, this list of conditions and the following disclaimer. */
/* */
/* * Redistributions in binary form must reproduce the above copyright */
/* notice, this list of conditions and the following disclaimer in the */
/* documentation and/or other materials provided with the distribution. */
/* */
/* * Neither the name of Texas Instruments Incorporated nor the names of */
/* its contributors may be used to endorse or promote products derived */
/* from this software without specific prior written permission. */
/* */
/* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */
/* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, */
/* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR */
/* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR */
/* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, */
/* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, */
/* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */
/* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, */
/* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR */
/* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, */
/* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */
/* ============================================================================ */
/******************************************************************************/
/* lnk_msp430f5659.cmd - LINKER COMMAND FILE FOR LINKING MSP430F5659 PROGRAMS */
/* */
/* Usage: lnk430 <obj files...> -o <out file> -m <map file> lnk.cmd */
/* cl430 <src files...> -z -o <out file> -m <map file> lnk.cmd */
/* */
/*----------------------------------------------------------------------------*/
/* These linker options are for command line linking only. For IDE linking, */
/* you should set your linker options in Project Properties */
/* -c LINK USING C CONVENTIONS */
/* -stack 0x0100 SOFTWARE STACK SIZE */
/* -heap 0x0100 HEAP AREA SIZE */
/* */
/*----------------------------------------------------------------------------*/
/* Version: 1.185 */
/*----------------------------------------------------------------------------*/
/****************************************************************************/
/* Specify the system memory map */
/****************************************************************************/
MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
RAM : origin = 0x2400, length = 0x4000
RAM2 : origin = 0xF0000, length = 0xC000
USBRAM : origin = 0x1C00, length = 0x0800
INFOA : origin = 0x1980, length = 0x0080
INFOB : origin = 0x1900, length = 0x0080
INFOC : origin = 0x1880, length = 0x0080
INFOD : origin = 0x1800, length = 0x0080
FLASH : origin = 0x8000, length = 0x7F80
FLASH2 : origin = 0x10000,length = 0x78000
INT00 : origin = 0xFF80, length = 0x0002
INT01 : origin = 0xFF82, length = 0x0002
INT02 : origin = 0xFF84, length = 0x0002
INT03 : origin = 0xFF86, length = 0x0002
INT04 : origin = 0xFF88, length = 0x0002
INT05 : origin = 0xFF8A, length = 0x0002
INT06 : origin = 0xFF8C, length = 0x0002
INT07 : origin = 0xFF8E, length = 0x0002
INT08 : origin = 0xFF90, length = 0x0002
INT09 : origin = 0xFF92, length = 0x0002
INT10 : origin = 0xFF94, length = 0x0002
INT11 : origin = 0xFF96, length = 0x0002
INT12 : origin = 0xFF98, length = 0x0002
INT13 : origin = 0xFF9A, length = 0x0002
INT14 : origin = 0xFF9C, length = 0x0002
INT15 : origin = 0xFF9E, length = 0x0002
INT16 : origin = 0xFFA0, length = 0x0002
INT17 : origin = 0xFFA2, length = 0x0002
INT18 : origin = 0xFFA4, length = 0x0002
INT19 : origin = 0xFFA6, length = 0x0002
INT20 : origin = 0xFFA8, length = 0x0002
INT21 : origin = 0xFFAA, length = 0x0002
INT22 : origin = 0xFFAC, length = 0x0002
INT23 : origin = 0xFFAE, length = 0x0002
INT24 : origin = 0xFFB0, length = 0x0002
INT25 : origin = 0xFFB2, length = 0x0002
INT26 : origin = 0xFFB4, length = 0x0002
INT27 : origin = 0xFFB6, length = 0x0002
INT28 : origin = 0xFFB8, length = 0x0002
INT29 : origin = 0xFFBA, length = 0x0002
INT30 : origin = 0xFFBC, length = 0x0002
INT31 : origin = 0xFFBE, length = 0x0002
INT32 : origin = 0xFFC0, length = 0x0002
INT33 : origin = 0xFFC2, length = 0x0002
INT34 : origin = 0xFFC4, length = 0x0002
INT35 : origin = 0xFFC6, length = 0x0002
INT36 : origin = 0xFFC8, length = 0x0002
INT37 : origin = 0xFFCA, length = 0x0002
INT38 : origin = 0xFFCC, length = 0x0002
INT39 : origin = 0xFFCE, length = 0x0002
INT40 : origin = 0xFFD0, length = 0x0002
INT41 : origin = 0xFFD2, length = 0x0002
INT42 : origin = 0xFFD4, length = 0x0002
INT43 : origin = 0xFFD6, length = 0x0002
INT44 : origin = 0xFFD8, length = 0x0002
INT45 : origin = 0xFFDA, length = 0x0002
INT46 : origin = 0xFFDC, length = 0x0002
INT47 : origin = 0xFFDE, length = 0x0002
INT48 : origin = 0xFFE0, length = 0x0002
INT49 : origin = 0xFFE2, length = 0x0002
INT50 : origin = 0xFFE4, length = 0x0002
INT51 : origin = 0xFFE6, length = 0x0002
INT52 : origin = 0xFFE8, length = 0x0002
INT53 : origin = 0xFFEA, length = 0x0002
INT54 : origin = 0xFFEC, length = 0x0002
INT55 : origin = 0xFFEE, length = 0x0002
INT56 : origin = 0xFFF0, length = 0x0002
INT57 : origin = 0xFFF2, length = 0x0002
INT58 : origin = 0xFFF4, length = 0x0002
INT59 : origin = 0xFFF6, length = 0x0002
INT60 : origin = 0xFFF8, length = 0x0002
INT61 : origin = 0xFFFA, length = 0x0002
INT62 : origin = 0xFFFC, length = 0x0002
RESET : origin = 0xFFFE, length = 0x0002
}
/****************************************************************************/
/* Specify the sections allocation into memory */
/****************************************************************************/
SECTIONS
{
.bss : {} > RAM | RAM2 /* Global & static vars */
.data : {} > RAM | RAM2 /* Global & static vars */
.TI.noinit : {} > RAM | RAM2 /* For #pragma noinit */
.sysmem : {} > RAM /* Dynamic memory allocation area */
.stack : {} > RAM (HIGH) /* Software system stack */
#ifndef __LARGE_DATA_MODEL__
.text : {} > FLASH /* Code */
#else
.text : {} >> FLASH2 | FLASH /* Code */
#endif
.text:_isr : {} > FLASH /* ISR Code space */
.cinit : {} > FLASH | FLASH2 /* Initialization tables - modified by Boaz (was only FLASH) */
#ifndef __LARGE_DATA_MODEL__
.const : {} > FLASH /* Constant data */
#else
.const : {} >> FLASH | FLASH2 /* Constant data */
#endif
.cio : {} > RAM /* C I/O Buffer */
.pinit : {} > FLASH /* C++ Constructor tables */
.binit : {} > FLASH /* Boot-time Initialization tables */
.init_array : {} > FLASH /* C++ Constructor tables */
.mspabi.exidx : {} > FLASH /* C++ Constructor tables */
.mspabi.extab : {} > FLASH /* C++ Constructor tables */
#ifdef __TI_COMPILER_VERSION
#if __TI_COMPILER_VERSION >= 15009000
#ifndef __LARGE_DATA_MODEL__
.TI.ramfunc : {} load=FLASH, run=RAM, table(BINIT)
#else
.TI.ramfunc : {} load=FLASH | FLASH2, run=RAM, table(BINIT)
#endif
#endif
#endif
.infoA : {} > INFOA /* MSP430 INFO FLASH Memory segments */
.infoB : {} > INFOB
.infoC : {} > INFOC
.infoD : {} > INFOD
/* MSP430 Interrupt vectors */
.int00 : {} > INT00
.int01 : {} > INT01
.int02 : {} > INT02
.int03 : {} > INT03
.int04 : {} > INT04
.int05 : {} > INT05
.int06 : {} > INT06
.int07 : {} > INT07
.int08 : {} > INT08
.int09 : {} > INT09
.int10 : {} > INT10
.int11 : {} > INT11
.int12 : {} > INT12
.int13 : {} > INT13
.int14 : {} > INT14
.int15 : {} > INT15
.int16 : {} > INT16
.int17 : {} > INT17
.int18 : {} > INT18
.int19 : {} > INT19
.int20 : {} > INT20
.int21 : {} > INT21
.int22 : {} > INT22
.int23 : {} > INT23
.int24 : {} > INT24
.int25 : {} > INT25
.int26 : {} > INT26
.int27 : {} > INT27
.int28 : {} > INT28
.int29 : {} > INT29
.int30 : {} > INT30
.int31 : {} > INT31
.int32 : {} > INT32
.int33 : {} > INT33
.int34 : {} > INT34
USCI_B2 : { * ( .int35 ) } > INT35 type = VECT_INIT
USCI_A2 : { * ( .int36 ) } > INT36 type = VECT_INIT
PORT4 : { * ( .int37 ) } > INT37 type = VECT_INIT
PORT3 : { * ( .int38 ) } > INT38 type = VECT_INIT
TIMER2_A1 : { * ( .int39 ) } > INT39 type = VECT_INIT
TIMER2_A0 : { * ( .int40 ) } > INT40 type = VECT_INIT
DAC12 : { * ( .int41 ) } > INT41 type = VECT_INIT
RTC : { * ( .int42 ) } > INT42 type = VECT_INIT
.int43 : {} > INT43
PORT2 : { * ( .int44 ) } > INT44 type = VECT_INIT
USCI_B1 : { * ( .int45 ) } > INT45 type = VECT_INIT
USCI_A1 : { * ( .int46 ) } > INT46 type = VECT_INIT
PORT1 : { * ( .int47 ) } > INT47 type = VECT_INIT
TIMER1_A1 : { * ( .int48 ) } > INT48 type = VECT_INIT
TIMER1_A0 : { * ( .int49 ) } > INT49 type = VECT_INIT
DMA : { * ( .int50 ) } > INT50 type = VECT_INIT
USB_UBM : { * ( .int51 ) } > INT51 type = VECT_INIT
TIMER0_A1 : { * ( .int52 ) } > INT52 type = VECT_INIT
TIMER0_A0 : { * ( .int53 ) } > INT53 type = VECT_INIT
ADC12 : { * ( .int54 ) } > INT54 type = VECT_INIT
USCI_B0 : { * ( .int55 ) } > INT55 type = VECT_INIT
USCI_A0 : { * ( .int56 ) } > INT56 type = VECT_INIT
WDT : { * ( .int57 ) } > INT57 type = VECT_INIT
TIMER0_B1 : { * ( .int58 ) } > INT58 type = VECT_INIT
TIMER0_B0 : { * ( .int59 ) } > INT59 type = VECT_INIT
COMP_B : { * ( .int60 ) } > INT60 type = VECT_INIT
UNMI : { * ( .int61 ) } > INT61 type = VECT_INIT
SYSNMI : { * ( .int62 ) } > INT62 type = VECT_INIT
.reset : {} > RESET /* MSP430 Reset vector */
}
/****************************************************************************/
/* Include peripherals memory map */
/****************************************************************************/
-l msp430f5659.cmd