Other Parts Discussed in Thread: DP83640
I am working on AM335x running on linux-3.0
I want to synchronize the CPU clock using the GPS clock which outputs PTP packets over Network.
Basically I want to implement PTP protocol on Linux so that slave device get sync to GPS Mater clock.
Does AM335x support PTP IEEE 1588 protocol ?
If yes are this configuration enough
- Select PPS Support - Device Drivers ---> PPS Support ---> <*> PPS Support
- Select PTP Clock Support - Device Drivers ---> PTP Clock Support ---> <*> PTP Clock Support
- Select TI CPTS PTP Clock - Device Drivers ---> PTP Clock Support ---> <*> TI CPTS as PTP clock
from the following post
Do I need this device DP83640 IEEE 1588 Precision Time Protocol Transceiver ?