This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 Simulator

Hi!

I am trying to configure the EDMA3 for a data transfer on C6748 Simulator(using CCSv5.5.0).

I am using the starterware "C6748_StarterWare_1_20_03_03". Here I am trying to trigger the transfer in a manual mode by writing to ESR.

But here in spite of writing to ESR, there is no transfer seen.

Here I configured the channel 0 in DMA mode. Tried both by enabling shadow and without it.

Also upon writing to a bit in EMCR register doesn't the corresponding bit in EMR. 

I need to ask, am I missing some steps in configuring the EDMA3, if so where do I debug the issue.

And I am trying to simulate this EDMA3 transfer on C6748 simulator. The general settings for this project are:

variant: Generic C674x Device

compiler version TIv7.4.4

Runtime support lib: rts6740.lib

And Target Config:

Connection:Texas instrument Simulator

Device: C674x CPU Accurate Simulator, Little Endian

Thanks in Advance