Hi
I have built few custom diag apps for our custom design now i want to test those on custom hardware, after putting all necessary boot images(MLO and app) and test apps on SDcard,when i insert SDcard on EVM booting and apps are working fine but the same SDcard not working on custom board so i came to know that we should create custom board library for our board.Initially i tried by following link but no clarity on this
http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_Board_Support#Creating
Note: Since our custom board DDR and UART design is same (pinmuxing) as EVM because of this i initially planed to do without custom board library, my understanding is atleast it has to boot at first stage with following logs
**** PDK SBL ****
**** Copying Application Image to DDR ****
SD Boot - file open completed successfully
MPU CPU0 image load completed
DSP1 image load completed
DSP2 image load completed
Jumping to MPU CPU0 Application...
main starts
Task_create OK
Enter FATFS_init
Enter FATFS_open
Enter Ipc_start
Ipc_start OK
DSP1 is attached
DSP2 is attached
HeapBufMP_create (HOST @ 0x81888850) OK
MessageQ_registerHeap OK
Message pointer table created OKMessages created OK
max_core = 2
MessageQ name (core0_queue) created OK
MessageQ name (core1_queue) created OK
MessageQ name (core2_queue) created OK
MessageQ name (core3_queue) created OK
mc_process_init OK
ipc_heap_init OK
IPC HOST is ready
0:>
But this is not happening in custom hardware, please explain how i can i resolve this. And the link is not clearing to me please guide its become blockage in my task.
BR,
Chethan