Hi,
I am trying to boot my from custom board using AM5726.
Below is my debug output while booting from SD card. I am using the pre-built image for GP EVM.
Could this be hardware issue? Do I need to rebuilt the SDK for AM5726?
Regards,
Hein
U-Boot SPL 2016.05-00118-gdd926c6-dirty (Nov 17 2016 - 11:57:28)
DRA752-GP ES2.0
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
No matching DT out of these options:
am57xx-beagle-x15
am572x-idk
am571x-idk
Failed to mount ext2 filesystem...
spl_load_image_ext_os: ext4fs mount err - 0
Failed to mount ext2 filesystem...
spl_load_image_ext: ext4fs mount err - 0