Hi,
I am having problems connecting our board to the network via DHCP. The board has a slight variation to the EVM unit where we are using a Marvell PHY device.
The uImage has been set to load the Marvell Device drivers and the Davinci Emac.
When the board is connected to a DHCP network, it sends out a DHCP DISCOVER packet but never sends a DHCP REQUEST.
This board has been booting using DHCP on the PSP Kernel release, thou we need to use the Montavista Kernel as it compiles with Gstreamer.
Has anyone else experianced this problem?
Thanks