Hi all,
I am having Spectrum Digital's C6474 EVM (REV D).
I downloaded the NDK 2.1.0 from TI website and compiled the Helloworld project after resolving some linker issue to find the csl_C6474.lib.
I am not able to transfer the packets.
When I load the helloworld application and run the application, I get the following output:
TCP/IP Stack 'Hello World!' Application
MAC Address read from EFUSE: 3c-2d-b7-18-14-c2
Core Number on which NDK is running = 0
EFUSED MAC Address = 3c-2d-b7-18-14-c2
Only on CORE 0: SGMII reset successful........
Only on CORE 0: SGMII config successful........
Only on CORE 0: SerDes should be up and running
EMAC has been started successfully
Registeration of the EMAC Successful
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Link Status: 100Mb/s Full Duplex on PHY 1
Then after, I get DHCP fault message. When I tried using static IP, I am not able to ping the board.
Have I missed any thing?
Your help is highly appreciated.
Thanks,
Amitkumar Solanki
(amitkumar.solanki@einfochips.com)