Hi,
We are using AM3352 Processor with DDR3 Memory(2nos)..
We are following the 6 layer Stack up as below.
L1 | TOP |
L2 | GND |
L3 | SIG |
L4 | SIG |
L5 | GND\VCC |
L6 | SIG |
When we route the DDR3 signal in L4 and L6 in that case it gets the reference of L5 and when route in L1 and L3 in that case it get reference of L2.
In L5 +1.5V plane is created which covered the DDR3 area so the the routing in L4 and L6 of DDR3 traces get reference of +1.5V and route of L1 and L4 get reference of GND.
So Is it OK to route DDR3 signals with different reference of +1.5V and GND?
Is there affected on RE and Functionality?