Hi,
We are using CCS V6.2 o develop RTOS for TM4C1294NCPDT, but in the release not of the host support section windows 10 is not mentioned can pls clarify the TIRtOS supporting condition to windows 10 OS host.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using CCS V6.2 o develop RTOS for TM4C1294NCPDT, but in the release not of the host support section windows 10 is not mentioned can pls clarify the TIRtOS supporting condition to windows 10 OS host.
TI-RTOS is target side software which has no Windows 10 dependency. If you see an issue that would be with the tools/or CCS plug-ins with logging, ROV etc. when running Windows 10, and that would be specific bugs that would need to be addressed but it looks like you are not seeing an issue, and the generic answer is: Yes it supports Windows 10