Hi,
I would like to do the following tests on TMDSICE3359 as eCAT master and TMDSIDK437x as eCAT slave:
1) Latency
2) Throughput
I would like to test with slave sending 128/256 bytes of data to the master.
My questions:
1) Once TMDSIDK437x receives eCAT broadcast frames from the master, how to send known 128/256 bytes on to the eCAT telegraph frames to the master? Can I get a working project as an example which does a similar functionality?
2) I am planning to change the cycle time from the default 2msec to 100usec to test latency and throughput: How to measure this performance via wireshark? Do you have any docs to test the performance?
Thanks.