This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x Starter Kit GPIO and PWM

Hi,


I would like to use the pins of the J10 header of the development board AM437x Starter Kit, but i am not having any success configuring the pins.

In order to configure the pins i add the following to .../arch/arm/boot/dts/am437x-gp-evm.dts

	hardware_pins: hardware_pins {
		pinctrl-single,pins = <
			0x000 MUX_MODE7		  /* gpmc_ap0.gpi01_0 */
			0x150 MUX_MODE7		  /* spi0_sclk.gpi0_2 */
			0x1A0 MUX_MODE9		  /* mcasp0_aclkr.gpi0_18 */
			0x1AC MUX_MODE9		  /* mcasp0_ahclkx.gpi0_3 */
			0x1A8 MUX_MODE9		  /* mcasp0_axr1.gpi0_2 */
			0x1A4 MUX_MODE9		  /* mcasp0_fsr.gpi0_19 */
			0x26C MUX_MODE9		  /* spi2c_cs0.gpi0_23 */
			0x264 MUX_MODE9		  /* spi2_d0.gpi0_20 */
			0x268 MUX_MODE9		  /* spi2_d1.gpi0_21 */
			0x260 MUX_MODE9		  /* spi2_sclk.gpi0_22 */
		>;
	};

here is the complete file:

/*
 * Copyright (C) 2013 Texas Instruments Incorporated - http://www.ti.com/
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */

/* AM437x GP EVM */

/dts-v1/;

#include "am4372.dtsi"
#include <dt-bindings/pinctrl/am43xx.h>
#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/interrupt-controller/irq.h>

/ {
	model = "TI AM437x GP EVM";
	compatible = "ti,am437x-gp-evm","ti,am4372","ti,am43";

	aliases {
		display0 = &lcd0;
		serial3 = &uart3;
	};

	evm_v3_3d: fixedregulator-v3_3d {
		compatible = "regulator-fixed";
		regulator-name = "evm_v3_3d";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		enable-active-high;
	};

	vtt_fixed: fixedregulator-vtt {
		compatible = "regulator-fixed";
		regulator-name = "vtt_fixed";
		regulator-min-microvolt = <1500000>;
		regulator-max-microvolt = <1500000>;
		regulator-always-on;
		regulator-boot-on;
		enable-active-high;
		gpio = <&gpio5 7 GPIO_ACTIVE_HIGH>;
	};

	vmmcwl_fixed: fixedregulator-mmcwl {
		compatible = "regulator-fixed";
		regulator-name = "vmmcwl_fixed";
		regulator-min-microvolt = <1800000>;
		regulator-max-microvolt = <1800000>;
		gpio = <&gpio1 20 GPIO_ACTIVE_HIGH>;
		startup-delay-us = <70000>;
		enable-active-high;
	};

	lcd_bl: backlight {
		compatible = "pwm-backlight";
		pwms = <&ecap0 0 50000 PWM_POLARITY_INVERTED>;
		brightness-levels = <0 51 53 56 62 75 101 152 255>;
		default-brightness-level = <8>;
	};

	matrix_keypad: matrix_keypad@0 {
		compatible = "gpio-matrix-keypad";
		debounce-delay-ms = <5>;
		col-scan-delay-us = <2>;

		pinctrl-names = "default", "sleep";
		pinctrl-0 = <&matrix_keypad_default>;
		pinctrl-1 = <&matrix_keypad_sleep>;

		linux,wakeup;

		row-gpios = <&gpio0 3 GPIO_ACTIVE_HIGH /* Bank0, pin3 */
				&gpio4 3 GPIO_ACTIVE_HIGH /* Bank4, pin3 */
				&gpio4 2 GPIO_ACTIVE_HIGH>; /* Bank4, pin2 */

		col-gpios = <&gpio3 19 GPIO_ACTIVE_HIGH /* Bank3, pin19 */
				&gpio3 20 GPIO_ACTIVE_HIGH>; /* Bank3, pin20 */

		linux,keymap = <0x00000201      /* P1 */
				0x00010202      /* P2 */
				0x01000067      /* UP */
				0x0101006a      /* RIGHT */
				0x02000069      /* LEFT */
				0x0201006c>;      /* DOWN */
		};

	lcd0: display {
		compatible = "osddisplays,osd057T0559-34ts", "panel-dpi";
		label = "lcd";

		panel-timing {
			clock-frequency = <33000000>;
			hactive = <800>;
			vactive = <480>;
			hfront-porch = <210>;
			hback-porch = <16>;
			hsync-len = <30>;
			vback-porch = <10>;
			vfront-porch = <22>;
			vsync-len = <13>;
			hsync-active = <0>;
			vsync-active = <0>;
			de-active = <1>;
			pixelclk-active = <1>;
		};

		port {
			lcd_in: endpoint {
				remote-endpoint = <&dpi_out>;
			};
		};
	};

	kim {
		compatible = "kim";
		nshutdown_gpio = <48>; /* Bank1, pin16 */
		dev_name = "/dev/ttyS3";
		flow_cntrl = <1>;
		baud_rate = <3000000>;
	};

	btwilink {
		compatible = "btwilink";
	};

	sound0: sound@0 {
		compatible = "simple-audio-card";
		simple-audio-card,name = "AM437x-GP-EVM";
		simple-audio-card,widgets =
			"Headphone", "Headphone Jack",
			"Line", "Line In";
		simple-audio-card,routing =
			"Headphone Jack",	"HPLOUT",
			"Headphone Jack",	"HPROUT",
			"LINE1L",		"Line In",
			"LINE1R",		"Line In";
		simple-audio-card,format = "dsp_b";
		simple-audio-card,bitclock-master = <&link0_codec>;
		simple-audio-card,frame-master = <&link0_codec>;
		simple-audio-card,bitclock-inversion;

		simple-audio-card,cpu {
			sound-dai = <&mcasp1>;
			system-clock-frequency = <12000000>;
		};

		link0_codec: simple-audio-card,codec {
			sound-dai = <&tlv320aic3106>;
			system-clock-frequency = <12000000>;
		};
	};
};

&am43xx_pinmux {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&wlan_pins_default &lcd_pins &ddr3_vtt_toggle_default &debugss_pins &unused_pins &board_pins &hardware_pins>;
	pinctrl-1 = <&wlan_pins_sleep>;

	ddr3_vtt_toggle_default: ddr_vtt_toggle_default {
		pinctrl-single,pins = <
			0x25C (DS0_PULL_UP_DOWN_EN | PIN_OUTPUT_PULLUP | DS0_FORCE_OFF_MODE | MUX_MODE7) /* spi0_cs0.gpio5_7 */
		>;
	};

	i2c0_pins: i2c0_pins {
		pinctrl-single,pins = <
			0x188 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)  /* i2c0_sda.i2c0_sda */
			0x18c (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)  /* i2c0_scl.i2c0_scl */
		>;
	};

	i2c1_pins_default: i2c1_pins_default {
		pinctrl-single,pins = <
			0x15c (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2)  /* spi0_cs0.i2c1_scl */
			0x158 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2)  /* spi0_d1.i2c1_sda  */
		>;
	};

	i2c1_pins_sleep: i2c1_pins_sleep {
		pinctrl-single,pins = <
			0x15c (PIN_INPUT_PULLUP | MUX_MODE7)
			0x158 (PIN_INPUT_PULLUP | MUX_MODE7)
		>;
	};

	mmc1_pins: pinmux_mmc1_pins {
		pinctrl-single,pins = <
			0x100 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_clk.mmc0_clk */
			0x104 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_cmd.mmc0_cmd */
			0x0f0 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat0.mmc0_dat0 */
			0x0f4 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat1.mmc0_dat1 */
			0x0f8 (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat2.mmc0_dat2 */
			0x0fc (PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat3.mmc0_dat3 */
			0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
		>;
	};

	mmc1_sleep_pins: pinmux_mmc1_sleep_pins {
		pinctrl-single,pins = <
			0x100 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x104 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x0f0 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x0f4 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x0f8 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x0fc (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x160 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
		>;
	};

	emmc_pins_default: emmc_pins_default {
		pinctrl-single,pins = <
			0x00 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad0.mmc1_dat0 */
			0x04 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad1.mmc1_dat1 */
			0x08 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad2.mmc1_dat2 */
			0x0c (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad3.mmc1_dat3 */
			0x10 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad4.mmc1_dat4 */
			0x14 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad5.mmc1_dat5 */
			0x18 (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad6.mmc1_dat6 */
			0x1c (PIN_INPUT_PULLUP | MUX_MODE1) /* gpmc_ad7.mmc1_dat7 */
			0x80 (PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_csn1.mmc1_clk */
			0x84 (PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_csn2.mmc1_cmd */
		>;
	};

	emmc_pins_sleep: emmc_pins_sleep {
		pinctrl-single,pins = <
			0x00 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad0.gpio1_0 */
			0x04 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad1.gpio1_1 */
			0x08 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad2.gpio1_2 */
			0x0c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad3.gpio1_3 */
			0x10 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad4.gpio1_4 */
			0x14 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad5.gpio1_5 */
			0x18 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad6.gpio1_6 */
			0x1c (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_ad7.gpio1_7 */
			0x80 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_csn1.gpio1_30 */
			0x84 (PIN_INPUT_PULLDOWN | MUX_MODE7) /* gpmc_csn2.gpio1_31 */
		>;
	};


	ecap0_pins_default: backlight_pins_default {
		pinctrl-single,pins = <
			0x164 MUX_MODE0       /* eCAP0_in_PWM0_out.eCAP0_in_PWM0_out MODE0 */
		>;
	};

	ecap0_pins_sleep: backlight_pins_sleep {
		pinctrl-single,pins = <
			0x164 (PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};

	pixcir_ts_pins_default: pixcir_ts_pins_default {
		pinctrl-single,pins = <
			0x264 (PIN_INPUT_PULLUP | MUX_MODE7)  /* spi2_d0.gpio3_22 */
		>;
	};

	pixcir_ts_pins_sleep: pixcir_ts_pins_sleep {
		pinctrl-single,pins = <
			0x264 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)  /* spi2_d0.gpio3_22 */
		>;
	};

	cpsw_default: cpsw_default {
		pinctrl-single,pins = <
			/* Slave 1 */
			0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txen.rgmii1_txen */
			0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxdv.rgmii1_rxctl */
			0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd1.rgmii1_txd3 */
			0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd0.rgmii1_txd2 */
			0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd1.rgmii1_txd1 */
			0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd0.rgmii1_txd0 */
			0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txclk.rmii1_tclk */
			0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxclk.rmii1_rclk */
			0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd1.rgmii1_rxd3 */
			0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd0.rgmii1_rxd2 */
			0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd1.rgmii1_rxd1 */
			0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd0.rgmii1_rxd0 */
		>;
	};

	cpsw_sleep: cpsw_sleep {
		pinctrl-single,pins = <
			/* Slave 1 reset value */
			0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x134 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x138 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x13c (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x140 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
		>;
	};

	davinci_mdio_default: davinci_mdio_default {
		pinctrl-single,pins = <
			/* MDIO */
			0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)	/* mdio_data.mdio_data */
			0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0)			/* mdio_clk.mdio_clk */
		>;
	};

	davinci_mdio_sleep: davinci_mdio_sleep {
		pinctrl-single,pins = <
			/* MDIO reset value */
			0x148 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x14c (PIN_INPUT | PULL_DISABLE | MUX_MODE7)
		>;
	};

	nand_flash_x8_default: nand_flash_x8_default {
		pinctrl-single,pins = <
			0x0  (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad0.gpmc_ad0 */
			0x4  (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad1.gpmc_ad1 */
			0x8  (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad2.gpmc_ad2 */
			0xc  (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad3.gpmc_ad3 */
			0x10 (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad4.gpmc_ad4 */
			0x14 (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad5.gpmc_ad5 */
			0x18 (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad6.gpmc_ad6 */
			0x1c (PIN_INPUT  | MUX_MODE0)	/* gpmc_ad7.gpmc_ad7 */
			0x70 (PIN_INPUT_PULLUP | MUX_MODE0)	/* gpmc_wait0.gpmc_wait0 */
			0x74 (PIN_OUTPUT_PULLUP | MUX_MODE7)	/* gpmc_wpn.gpmc_wpn */
			0x7c (PIN_OUTPUT | MUX_MODE0)		/* gpmc_csn0.gpmc_csn0  */
			0x90 (PIN_OUTPUT | MUX_MODE0)		/* gpmc_advn_ale.gpmc_advn_ale */
			0x94 (PIN_OUTPUT | MUX_MODE0)		/* gpmc_oen_ren.gpmc_oen_ren */
			0x98 (PIN_OUTPUT | MUX_MODE0)		/* gpmc_wen.gpmc_wen */
			0x9c (PIN_OUTPUT | MUX_MODE0)		/* gpmc_be0n_cle.gpmc_be0n_cle */
		>;
	};

	nand_flash_x8_sleep: nand_flash_x8_sleep {
		pinctrl-single,pins = <
			0x0  (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad0.gpmc_ad0 */
			0x4  (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad1.gpmc_ad1 */
			0x8  (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad2.gpmc_ad2 */
			0xc  (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad3.gpmc_ad3 */
			0x10 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad4.gpmc_ad4 */
			0x14 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad5.gpmc_ad5 */
			0x18 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad6.gpmc_ad6 */
			0x1c (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_ad7.gpmc_ad7 */
			0x70 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)	/* gpmc_wait0.gpmc_wait0 */
			0x74 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_wpn.gpmc_wpn */
			0x7c (PIN_INPUT | PULL_DISABLE | MUX_MODE7)		/* gpmc_csn0.gpmc_csn0  */
			0x90 (PIN_INPUT | PULL_DISABLE | MUX_MODE7)		/* gpmc_advn_ale.gpmc_advn_ale */
			0x94 (PIN_INPUT_PULLDOWN | MUX_MODE7)		/* gpmc_oen_ren.gpmc_oen_ren */
			0x98 (PIN_INPUT_PULLDOWN |  MUX_MODE7)		/* gpmc_wen.gpmc_wen */
			0x9c (PIN_INPUT | PULL_DISABLE | MUX_MODE7)		/* gpmc_be0n_cle.gpmc_be0n_cle */
		>;
	};

	dss_pinctrl_default: dss_pinctrl_default {
		pinctrl-single,pins = <
			0x020 (PIN_OUTPUT_PULLUP | MUX_MODE1) /*gpmc ad 8 -> DSS DATA 23 */
			0x024 (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x028 (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x02c (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x030 (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x034 (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x038 (PIN_OUTPUT_PULLUP | MUX_MODE1)
			0x03c (PIN_OUTPUT_PULLUP | MUX_MODE1) /*gpmc ad 15 -> DSS DATA 16 */
			0x0a0 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS DATA 0 */
			0x0a4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0a8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0ac (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0b0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0b4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0b8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0bc (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0c0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0c4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0c8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0cc (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0d0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0d4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0d8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
			0x0dc (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS DATA 15 */
			0x0e0 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS VSYNC */
			0x0e4 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS HSYNC */
			0x0e8 (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS PCLK */
			0x0ec (PIN_OUTPUT_PULLUP | MUX_MODE0) /* DSS AC BIAS EN */

		>;
	};

	dss_pinctrl_sleep: dss_pinctrl_sleep {
		pinctrl-single,pins = <
			0x020 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x024 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x028 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x02C (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x030 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x034 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x038 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x03C (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0A0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0A4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0A8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0AC (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0B0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0B4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0B8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0BC (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0C0 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0C4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0C8 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0CC (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0D0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0D4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0D8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | PULL_DISABLE | MUX_MODE7)
			0x0DC (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0E0 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0E4 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0E8 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x0EC (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};

	lcd_pins: lcd_pins {
		pinctrl-single,pins = <
			/* GPIO 5_8 to select LCD / HDMI */
			0x238 (PIN_OUTPUT_PULLUP | MUX_MODE7)
		>;
	};

	mmc3_pins_default: pinmux_mmc3_pins_default {
		pinctrl-single,pins = <
			0x8c (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_clk.mmc2_clk */
			0x88 (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_csn3.mmc2_cmd */
			0x44 (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_a1.mmc2_dat0 */
			0x48 (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_a2.mmc2_dat1 */
			0x4c (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_a3.mmc2_dat2 */
			0x78 (PIN_INPUT_PULLUP | MUX_MODE3)      /* gpmc_be1n.mmc2_dat3 */
		>;
	};

	mmc3_pins_sleep: pinmux_mmc3_pins_sleep {
		pinctrl-single,pins = <
			0x8c (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_clk.mmc2_clk */
			0x88 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_csn3.mmc2_cmd */
			0x44 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_a1.mmc2_dat0 */
			0x48 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_a2.mmc2_dat1 */
			0x4c (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_a3.mmc2_dat2 */
			0x78 (PIN_INPUT_PULLDOWN | MUX_MODE7)	/* gpmc_be1n.mmc2_dat3 */
		>;
	};

	wlan_pins_default: pinmux_wlan_pins_default {
		pinctrl-single,pins = <
			0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE7)		/* gpmc_a4.gpio1_20 WL_EN */
			0x5c (PIN_INPUT | WAKEUP_ENABLE | MUX_MODE7) 	/* gpmc_a7.gpio1_23 WL_IRQ*/
			0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE7)		/* gpmc_a0.gpio1_16 BT_EN*/
		>;
	};

	wlan_pins_sleep: pinmux_wlan_pins_sleep {
		pinctrl-single,pins = <
			0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE7)		/* gpmc_a4.gpio1_20 WL_EN */
			0x5c (PIN_INPUT | WAKEUP_ENABLE | MUX_MODE7) 	/* gpmc_a7.gpio1_23 WL_IRQ*/
			0x40 (PIN_OUTPUT_PULLUP | MUX_MODE7)		/* gpmc_a0.gpio1_16 BT_EN*/
		>;
	};

	uart3_pins: uart3_pins {
		pinctrl-single,pins = <
			0x228 (PIN_INPUT | MUX_MODE0) 		/* uart3_rxd.uart3_rxd */
			0x22c (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart3_txd.uart3_txd */
			0x230 (PIN_INPUT_PULLUP | MUX_MODE0) 	/* uart3_ctsn.uart3_ctsn */
			0x234 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart3_rtsn.uart3_rtsn */
		>;
	};

	dcan0_default: dcan0_default_pins {
		pinctrl-single,pins = <
			0x178 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* uart1_ctsn.d_can0_tx */
			0x17c (PIN_INPUT_PULLUP | MUX_MODE2) /* uart1_rtsn.d_can0_rx */
		>;
	};

	dcan1_default: dcan1_default_pins {
		pinctrl-single,pins = <
			0x180 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* uart1_rxd.d_can1_tx */
			0x184 (PIN_INPUT_PULLUP | MUX_MODE2) /* uart1_txd.d_can1_rx */
		>;
	};

	mcasp1_pins: mcasp1_pins {
		pinctrl-single,pins = <
			0x108 (PIN_OUTPUT_PULLDOWN | MUX_MODE4)	/* mii1_col.mcasp1_axr2 */
			0x10c (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* mii1_crs.mcasp1_aclkx */
			0x110 (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* mii1_rxerr.mcasp1_fsx */
			0x144 (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* rmii1_ref_clk.mcasp1_axr3 */
		>;
	};

	mcasp1_sleep_pins: mcasp1_sleep_pins {
		pinctrl-single,pins = <
			0x108 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x10c (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x110 (PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x144 (PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};

	vpfe0_pins_default: vpfe0_pins_default {
		pinctrl-single,pins = <
			0x1B0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_hd mode 0*/
			0x1B4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_vd mode 0*/
			0x1C0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_pclk mode 0*/
			0x1C4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data8 mode 0*/
			0x1C8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data9 mode 0*/
			0x208 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data0 mode 0*/
			0x20C (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data1 mode 0*/
			0x210 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data2 mode 0*/
			0x214 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data3 mode 0*/
			0x218 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data4 mode 0*/
			0x21C (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data5 mode 0*/
			0x220 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data6 mode 0*/
			0x224 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data7 mode 0*/
		>;
	};

	vpfe0_pins_sleep: vpfe0_pins_sleep {
		pinctrl-single,pins = <
			0x1B0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_hd mode 0*/
			0x1B4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_vd mode 0*/
			0x1C0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_pclk mode 0*/
			0x1C4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data8 mode 0*/
			0x1C8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data9 mode 0*/
			0x208 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data0 mode 0*/
			0x20C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data1 mode 0*/
			0x210 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data2 mode 0*/
			0x214 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data3 mode 0*/
			0x218 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data4 mode 0*/
			0x21C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data5 mode 0*/
			0x220 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data6 mode 0*/
			0x224 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data7 mode 0*/
		>;
	};

	vpfe1_pins_default: vpfe1_pins_default {
		pinctrl-single,pins = <
			0x1CC (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data9 mode 0*/
			0x1D0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data8 mode 0*/
			0x1D4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_hd mode 0*/
			0x1D8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_vd mode 0*/
			0x1DC (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_pclk mode 0*/
			0x1E8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data0 mode 0*/
			0x1EC (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data1 mode 0*/
			0x1F0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data2 mode 0*/
			0x1F4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data3 mode 0*/
			0x1F8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data4 mode 0*/
			0x1FC (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data5 mode 0*/
			0x200 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data6 mode 0*/
			0x204 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam1_data7 mode 0*/
		>;
	};

	vpfe1_pins_sleep: vpfe1_pins_sleep {
		pinctrl-single,pins = <
			0x1CC (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data9 mode 0*/
			0x1D0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data8 mode 0*/
			0x1D4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_hd mode 0*/
			0x1D8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_vd mode 0*/
			0x1DC (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_pclk mode 0*/
			0x1E8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data0 mode 0*/
			0x1EC (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data1 mode 0*/
			0x1F0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data2 mode 0*/
			0x1F4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data3 mode 0*/
			0x1F8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data4 mode 0*/
			0x1FC (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data5 mode 0*/
			0x200 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data6 mode 0*/
			0x204 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam1_data7 mode 0*/
		>;
	};

	uart0_pins_default: uart0_pins_default {
		pinctrl-single,pins = <
			0x168 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE0)
			0x16C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE0)
			0x170 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | DS0_PULL_UP_DOWN_EN | MUX_MODE0) /* uart0_rxd.uart0_rxd */
			0x174 (PIN_INPUT | PULL_DISABLE | SLEWCTRL_FAST | DS0_PULL_UP_DOWN_EN | MUX_MODE0) /* uart0_txd.uart0_txd */
		>;
	};

	uart0_pins_sleep: uart0_pins_sleep {
		pinctrl-single,pins = <
			0x168 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)
			0x16C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)
			0x170 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | DS0_PULL_UP_DOWN_EN | MUX_MODE0) /* uart0_rxd.uart0_rxd */
			0x174 (PIN_INPUT_PULLDOWN | SLEWCTRL_FAST | DS0_PULL_UP_DOWN_EN | MUX_MODE0) /* uart0_txd.uart0_txd */
		>;
	};

	matrix_keypad_default: matrix_keypad_default {
		pinctrl-single,pins = <
			0x1a4 (PIN_OUTPUT | MUX_MODE7)
			0x1a8 (PIN_OUTPUT | MUX_MODE7)
			0x1ac (PIN_INPUT | PULL_DISABLE | MUX_MODE9)	/* mcasp0_ahclkx.gpio0_3 */
		>;
	};

	matrix_keypad_sleep: matrix_keypad_sleep {
		pinctrl-single,pins = <
			0x1a4 (PULL_UP | MUX_MODE7)
			0x1a8 (PULL_UP | MUX_MODE7)
			0x1ac (PIN_INPUT | PULL_DISABLE | MUX_MODE9)
		>;
	};

	usb2_phy1_default: usb2_phy1_default {
		pinctrl-single,pins = <
			0x2c0 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE0)
		>;
	};

	usb2_phy1_sleep: usb2_phy1_sleep {
		pinctrl-single,pins = <
			0x2c0 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};

	usb2_phy2_default: usb2_phy2_default {
		pinctrl-single,pins = <
			0x2c4 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE0)
		>;
	};

	usb2_phy2_sleep: usb2_phy2_sleep {
		pinctrl-single,pins = <
			0x2c4 (DS0_PULL_UP_DOWN_EN | PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};

	debugss_pins: pinmux_debugss_pins {
		pinctrl-single,pins = <
			0x290 (PIN_INPUT_PULLDOWN)
			0x294 (PIN_INPUT_PULLDOWN)
			0x298 (PIN_INPUT_PULLDOWN)
			0x29C (PIN_INPUT_PULLDOWN)
			0x2A0 (PIN_INPUT_PULLDOWN)
			0x2A4 (PIN_INPUT_PULLDOWN)
			0x2A8 (PIN_INPUT_PULLDOWN)
		>;
	};

	board_pins: board_pins {
		pinctrl-single,pins = <
			0x26c (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* spi2_cs0.gpio3_25 SEL_eMMCorNANDn */
		>;
	};

	unused_pins: unused_pins {
		pinctrl-single,pins = <
			0x54	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x58	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x60	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x64	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x68	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x6C	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x150	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x154	(PIN_INPUT_PULLDOWN | MUX_MODE0)
			0x190	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x194	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x198	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x19C	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x1A0	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x23C	(PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x240	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x244	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x248	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x24C	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x250	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x254	(PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x258	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x260	(PIN_INPUT | PULL_DISABLE | MUX_MODE7)
			0x268	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x270	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x278	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x27C	(PIN_INPUT | PULL_DISABLE)
			0x2C8	(PIN_INPUT_PULLDOWN)
			0x2D4	(PIN_INPUT_PULLDOWN)
			0x2D8	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2DC	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2E0	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2E4	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2E8	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2EC	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2F0	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2F4	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2F8	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x2FC	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x300	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x304	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x308	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x30C	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x310	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x314	(PIN_INPUT_PULLDOWN | MUX_MODE7)
			0x318	(PIN_INPUT_PULLDOWN | MUX_MODE7)
		>;
	};
	
	hardware_pins: hardware_pins {
		pinctrl-single,pins = <
			0x000 MUX_MODE7		  /* gpmc_ap0.gpi01_0 */
			0x150 MUX_MODE7		  /* spi0_sclk.gpi0_2 */
			0x1A0 MUX_MODE9		  /* mcasp0_aclkr.gpi0_18 */
			0x1AC MUX_MODE9		  /* mcasp0_ahclkx.gpi0_3 */
			0x1A8 MUX_MODE9		  /* mcasp0_axr1.gpi0_2 */
			0x1A4 MUX_MODE9		  /* mcasp0_fsr.gpi0_19 */
			0x26C MUX_MODE9		  /* spi2c_cs0.gpi0_23 */
			0x264 MUX_MODE9		  /* spi2_d0.gpi0_20 */
			0x268 MUX_MODE9		  /* spi2_d1.gpi0_21 */
			0x260 MUX_MODE9		  /* spi2_sclk.gpi0_22 */
		>;
	};
};

&i2c0 {
	status = "okay";
	pinctrl-names = "default";
	pinctrl-0 = <&i2c0_pins>;
	clock-frequency = <100000>;

	tps65218: tps65218@24 {
		reg = <0x24>;
		compatible = "ti,tps65218";
		interrupts = <GIC_SPI 7 IRQ_TYPE_NONE>; /* NMIn */
		interrupt-parent = <&gic>;
		interrupt-controller;
		#interrupt-cells = <2>;

		dcdc1: regulator-dcdc1 {
			compatible = "ti,tps65218-dcdc1";
			regulator-name = "vdd_core";
			regulator-min-microvolt = <912000>;
			regulator-max-microvolt = <1144000>;
			regulator-boot-on;
			regulator-always-on;
		};

		dcdc2: regulator-dcdc2 {
			compatible = "ti,tps65218-dcdc2";
			regulator-name = "vdd_mpu";
			regulator-min-microvolt = <912000>;
			regulator-max-microvolt = <1378000>;
			regulator-boot-on;
			regulator-always-on;
		};

		dcdc3: regulator-dcdc3 {
			compatible = "ti,tps65218-dcdc3";
			regulator-name = "vdcdc3";
			regulator-min-microvolt = <1500000>;
			regulator-max-microvolt = <1500000>;
			regulator-boot-on;
			regulator-always-on;
			regulator-state-mem {
				regulator-on-in-suspend;
			};
			regulator-state-disk {
				regulator-off-in-suspend;
			};
		};

		dcdc5: regulator-dcdc5 {
			compatible = "ti,tps65218-dcdc5";
			regulator-name = "v1_0bat";
			regulator-min-microvolt = <1000000>;
			regulator-max-microvolt = <1000000>;
			regulator-boot-on;
			regulator-always-on;
			regulator-state-mem {
				regulator-on-in-suspend;
			};
		};

		dcdc6: regulator-dcdc6 {
			compatible = "ti,tps65218-dcdc6";
			regulator-name = "v1_8bat";
			regulator-min-microvolt = <1800000>;
			regulator-max-microvolt = <1800000>;
			regulator-boot-on;
			regulator-always-on;
			regulator-state-mem {
				regulator-on-in-suspend;
			};
		};

		ldo1: regulator-ldo1 {
			compatible = "ti,tps65218-ldo1";
			regulator-min-microvolt = <1800000>;
			regulator-max-microvolt = <1800000>;
			regulator-boot-on;
			regulator-always-on;
		};
	};

        ov2659@30 {
		compatible = "ti,ov2659";
		reg = <0x30>;

		port {
			ov2659_0: endpoint {
				remote-endpoint = <&vpfe1_ep>;
				mclk-frequency = <12000000>;
			};
		};
	};
};

&i2c1 {
	status = "okay";
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c1_pins_default>;
	pinctrl-1 = <&i2c1_pins_sleep>;
	pixcir_ts@5c {
		compatible = "pixcir,pixcir_tangoc";
		pinctrl-names = "default", "sleep";
		pinctrl-0 = <&pixcir_ts_pins_default>;
		pinctrl-1 = <&pixcir_ts_pins_sleep>;
		reg = <0x5c>;
		interrupt-parent = <&gpio3>;
		interrupts = <22 0>;

		attb-gpio = <&gpio3 22 GPIO_ACTIVE_HIGH>;

		interrupts-extended = <&gpio3 22 GPIO_ACTIVE_HIGH>,
				      <&am43xx_pinmux 0x264>;

		touchscreen-size-x = <1024>;
		touchscreen-size-y = <600>;
	};

	tlv320aic3106: tlv320aic3106@1b {
		#sound-dai-cells = <0>;
		compatible = "ti,tlv320aic3106";
		reg = <0x1b>;
		status = "okay";

		/* Regulators */
		IOVDD-supply = <&evm_v3_3d>; /* V3_3D -> <tps63031> EN: V1_8D -> VBAT */
		AVDD-supply = <&evm_v3_3d>; /* v3_3AUD -> V3_3D -> ... */
		DRVDD-supply = <&evm_v3_3d>; /* v3_3AUD -> V3_3D -> ... */
		DVDD-supply = <&ldo1>; /* V1_8D -> LDO1 */
	};

	ov2659@30 {
		compatible = "ti,ov2659";
		reg = <0x30>;

		port {
			ov2659_1: endpoint {
				remote-endpoint = <&vpfe0_ep>;
				mclk-frequency = <12000000>;
			};
		};
	};

};

&epwmss0 {
	status = "okay";
};

&tscadc {
        status = "okay";

        adc {
                ti,adc-channels = <0 1 2 3 4 5 6 7>;
        };
};

&ecap0 {
	status = "okay";
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&ecap0_pins_default>;
	pinctrl-1 = <&ecap0_pins_sleep>;
};

&gpio0 {
	status = "okay";
};

&gpio1 {
	status = "okay";
};

&gpio2 {
	status = "okay";
};

&gpio3 {
	status = "okay";
};

&gpio4 {
	status = "okay";
};

&gpio5 {
	status = "okay";
	ti,no-reset-on-init;
};

&mmc1 {
	status = "okay";
	vmmc-supply = <&evm_v3_3d>;
	bus-width = <4>;
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&mmc1_pins>;
	pinctrl-1 = <&mmc1_sleep_pins>;
	cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
};

/* eMMC sits on mmc2 */
&mmc2 {
	status = "disabled"; /* Disable GPMC/NAND when enabling mmc2 */
	vmmc-supply = <&evm_v3_3d>;
	bus-width = <8>;
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&emmc_pins_default>;
	pinctrl-1 = <&emmc_pins_sleep>;
	ti,non-removable;
};

&mmc3 {
	status = "okay";
	/*
	 * These are on the crossbar and are outlined in the
	 * xbar-event-map element. Using GPIO0 and GPIO1 direct
	 * mapped events.
	 */
	dmas = <&edma 22
		&edma 23>;
	dma-names = "tx", "rx";
	vmmc-supply = <&vmmcwl_fixed>;
	bus-width = <4>;
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&mmc3_pins_default>;
	pinctrl-1 = <&mmc3_pins_sleep>;
	cap-power-off-card;
	keep-power-in-suspend;
	ti,non-removable;

	#address-cells = <1>;
	#size-cells = <0>;
	wlcore: wlcore@0 {
		compatible = "ti,wlcore";
		reg = <2>;
		interrupt-parent = <&gpio1>;
		interrupts = <23 IRQ_TYPE_LEVEL_HIGH>;
	};
};

&edma {
	ti,edma-xbar-event-map = /bits/ 16 <1 22
					    2 23>;
};

&uart3 {
	status = "okay";
	pinctrl-names = "default";
	pinctrl-0 = <&uart3_pins>;
};

&dwc3_1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&usb2_phy1_default>;
	pinctrl-1 = <&usb2_phy1_sleep>;

};

&usb2_phy1 {
	status = "okay";
};

&usb1 {
	dr_mode = "otg";
	status = "okay";
};

&dwc3_2 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&usb2_phy2_default>;
	pinctrl-1 = <&usb2_phy2_sleep>;
};

&usb2_phy2 {
	status = "okay";
};

&usb2 {
	dr_mode = "host";
	status = "okay";
};

&mac {
	slaves = <1>;
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&cpsw_default>;
	pinctrl-1 = <&cpsw_sleep>;
	status = "okay";
};

&davinci_mdio {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&davinci_mdio_default>;
	pinctrl-1 = <&davinci_mdio_sleep>;
	status = "okay";
};

&cpsw_emac0 {
	phy_id = <&davinci_mdio>, <0>;
	phy-mode = "rgmii";
};

&elm {
	status = "okay";
};

&gpmc {
	status = "okay"; /* Disable eMMC when enabling GPMC/NAND */
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&nand_flash_x8_default>;
	pinctrl-1 = <&nand_flash_x8_sleep>;
	ranges = <0 0 0 0x01000000>;	/* minimum GPMC partition = 16MB */
	nand@0,0 {
		reg = <0 0 4>;		/* device IO registers */
		ti,nand-ecc-opt = "bch16";
		ti,elm-id = <&elm>;
		nand-bus-width = <8>;
		gpmc,device-width = <1>;
		gpmc,sync-clk-ps = <0>;
		gpmc,cs-on-ns = <0>;
		gpmc,cs-rd-off-ns = <40>;
		gpmc,cs-wr-off-ns = <40>;
		gpmc,adv-on-ns = <0>;
		gpmc,adv-rd-off-ns = <25>;
		gpmc,adv-wr-off-ns = <25>;
		gpmc,we-on-ns = <0>;
		gpmc,we-off-ns = <20>;
		gpmc,oe-on-ns = <3>;
		gpmc,oe-off-ns = <30>;
		gpmc,access-ns = <30>;
		gpmc,rd-cycle-ns = <40>;
		gpmc,wr-cycle-ns = <40>;
		gpmc,wait-pin = <0>;
		gpmc,bus-turnaround-ns = <0>;
		gpmc,cycle2cycle-delay-ns = <0>;
		gpmc,clk-activation-ns = <0>;
		gpmc,wait-monitoring-ns = <0>;
		gpmc,wr-access-ns = <40>;
		gpmc,wr-data-mux-bus-ns = <0>;
		/* MTD partition table */
		/* All SPL-* partitions are sized to minimal length
		 * which can be independently programmable. For
		 * NAND flash this is equal to size of erase-block */
		#address-cells = <1>;
		#size-cells = <1>;
		partition@0 {
			label = "NAND.SPL";
			reg = <0x00000000 0x00040000>;
		};
		partition@1 {
			label = "NAND.SPL.backup1";
			reg = <0x00040000 0x00040000>;
		};
		partition@2 {
			label = "NAND.SPL.backup2";
			reg = <0x00080000 0x00040000>;
		};
		partition@3 {
			label = "NAND.SPL.backup3";
			reg = <0x000c0000 0x00040000>;
		};
		partition@4 {
			label = "NAND.u-boot-spl-os";
			reg = <0x00100000 0x00080000>;
		};
		partition@5 {
			label = "NAND.u-boot";
			reg = <0x00180000 0x00100000>;
		};
		partition@6 {
			label = "NAND.u-boot-env";
			reg = <0x00280000 0x00040000>;
		};
		partition@7 {
			label = "NAND.u-boot-env.backup1";
			reg = <0x002c0000 0x00040000>;
		};
		partition@8 {
			label = "NAND.kernel";
			reg = <0x00300000 0x00700000>;
		};
		partition@9 {
			label = "NAND.file-system";
			reg = <0x00a00000 0x1f600000>;
		};
	};
};

&uart0 {
	status = "okay";
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&uart0_pins_default>;
	pinctrl-1 = <&uart0_pins_sleep>;
};

&dss {
	status = "ok";

	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&dss_pinctrl_default>;
	pinctrl-1 = <&dss_pinctrl_sleep>;

	port {
		dpi_out: endpoint@0 {
			remote-endpoint = <&lcd_in>;
			data-lines = <24>;
		};
	};
};

&dcan0 {
	pinctrl-names = "default";
	pinctrl-0 = <&dcan0_default>;
	status = "okay";
};

&dcan1 {
	pinctrl-names = "default";
	pinctrl-0 = <&dcan1_default>;
	status = "okay";
};

&mcasp1 {
	#sound-dai-cells = <0>;
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&mcasp1_pins>;
	pinctrl-1 = <&mcasp1_sleep_pins>;

	status = "okay";

	op-mode = <0>; /* MCASP_IIS_MODE */
	tdm-slots = <2>;
	/* 4 serializers */
	serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
		0 0 1 2
	>;
	tx-num-evt = <32>;
	rx-num-evt = <32>;
};

&cpu {
	cpu0-supply = <&dcdc2>;
};

&rtc {
        status = "okay";
};

&wkup_m3 {
	ti,set-io-isolation;
	ti,scale-data-fw = "am43x-evm-scale-data.bin";
};

&vpfe1 {
	status = "okay";
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&vpfe1_pins_default>;
	pinctrl-1 = <&vpfe1_pins_sleep>;

	/* Camera port */
	port {
		vpfe1_ep: endpoint {
			remote-endpoint = <&ov2659_0>;
			if_type = <2>;
			bus_width = <8>;
			hdpol = <0>;
			vdpol = <0>;
		};
	};
};

&vpfe0 {
	status = "okay";
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&vpfe0_pins_default>;
	pinctrl-1 = <&vpfe0_pins_sleep>;

	/* Camera port */
	port {
		vpfe0_ep: endpoint {
			remote-endpoint = <&ov2659_1>;
			if_type = <2>;
			bus_width = <8>;
			hdpol = <0>;
			vdpol = <0>;
		};
	};
};

Then i tried to compile this file using the command:
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- am437x-gp-evm.dtb

Copied the am437x-gp-evm.dtb to targetfilesystem/boot

Finally, while trying to define the pin values under /sys/class/gpio i couldn't get the right value on the J10 connector.

Could anyone explain me the right way to configure the pins multiplexer and how to activate the pwm modules? An example will be fantastic.


Thanks,

Pedro

  • The software team have been notified. They will respond here.
  • I already got control over the above pins, including the PWM. It was needed to change the /boot/uEnv.txt file.

    fdtfile=am437x-sk-evm_new.dtb

    And i have change the .dts file like this:

    /*
     * Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    /* AM437x SK EVM */
    
    /dts-v1/;
    
    #include "am4372.dtsi"
    #include <dt-bindings/pinctrl/am43xx.h>
    #include <dt-bindings/pwm/pwm.h>
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/input/input.h>
    
    / {
    	model = "TI AM437x SK EVM";
    	compatible = "ti,am437x-sk-evm","ti,am4372","ti,am43";
    
    	aliases {
    		display0 = &lcd0;
    	};
    
    	backlight {
    		compatible = "pwm-backlight";
    		pwms = <&ecap0 0 50000 PWM_POLARITY_INVERTED>;
    		brightness-levels = <0 51 53 56 62 75 101 152 255>;
    		default-brightness-level = <8>;
    	};
    
    	sound {
    		compatible = "simple-audio-card";
    		simple-audio-card,name = "AM437x-SK-EVM";
    		simple-audio-card,widgets =
    			"Headphone", "Headphone Jack";
    		simple-audio-card,routing =
    			"Headphone Jack",	"HPLOUT",
    			"Headphone Jack",	"HPROUT";
    		simple-audio-card,format = "dsp_b";
    		simple-audio-card,bitclock-master = <&sound_master>;
    		simple-audio-card,frame-master = <&sound_master>;
    		simple-audio-card,bitclock-inversion;
    
    		simple-audio-card,cpu {
    			sound-dai = <&mcasp1>;
    		};
    
    		sound_master: simple-audio-card,codec {
    			sound-dai = <&tlv320aic3106>;
    			system-clock-frequency = <24000000>;
    		};
    	};
    
    	matrix_keypad: matrix_keypad@0 {
    		compatible = "gpio-matrix-keypad";
    
    		pinctrl-names = "default";
    		pinctrl-0 = <&matrix_keypad_pins>;
    
    		debounce-delay-ms = <5>;
    		col-scan-delay-us = <5>;
    
    		row-gpios = <&gpio5 5 GPIO_ACTIVE_HIGH		/* Bank5, pin5 */
    				&gpio5 6 GPIO_ACTIVE_HIGH>;	/* Bank5, pin6 */
    
    		col-gpios = <&gpio5 13 GPIO_ACTIVE_HIGH		/* Bank5, pin13 */
    				&gpio5 4 GPIO_ACTIVE_HIGH>;	/* Bank5, pin4 */
    
    		linux,keymap = <
    				MATRIX_KEY(0, 0, KEY_DOWN)
    				MATRIX_KEY(0, 1, KEY_RIGHT)
    				MATRIX_KEY(1, 0, KEY_LEFT)
    				MATRIX_KEY(1, 1, KEY_UP)
    			>;
    	};
    
    	leds {
    		compatible = "gpio-leds";
    
    		pinctrl-names = "default";
    		pinctrl-0 = <&leds_pins>;
    
    		led@0 {
    			label = "am437x-sk:red:heartbeat";
    			gpios = <&gpio5 0 GPIO_ACTIVE_HIGH>;	/* Bank 5, pin 0 */
    			linux,default-trigger = "heartbeat";
    			default-state = "off";
    		};
    
    		led@1 {
    			label = "am437x-sk:green:mmc1";
    			gpios = <&gpio5 1 GPIO_ACTIVE_HIGH>;	/* Bank 5, pin 1 */
    			linux,default-trigger = "mmc0";
    			default-state = "off";
    		};
    
    		led@2 {
    			label = "am437x-sk:blue:cpu0";
    			gpios = <&gpio5 2 GPIO_ACTIVE_HIGH>;	/* Bank 5, pin 2 */
    			linux,default-trigger = "cpu0";
    			default-state = "off";
    		};
    
    		led@3 {
    			label = "am437x-sk:blue:usr3";
    			gpios = <&gpio5 3 GPIO_ACTIVE_HIGH>;	/* Bank 5, pin 3 */
    			default-state = "off";
    		};
    	};
    
    	lcd0: display {
    		compatible = "newhaven,nhd-4.3-480272ef-atxl", "panel-dpi";
    		label = "lcd";
    
    		pinctrl-names = "default";
    		pinctrl-0 = <&lcd_pins>;
    
    		enable-gpios = <&gpio1 7 GPIO_ACTIVE_HIGH>;
    
    		panel-timing {
    			clock-frequency = <9000000>;
    			hactive = <480>;
    			vactive = <272>;
    			hfront-porch = <2>;
    			hback-porch = <2>;
    			hsync-len = <41>;
    			vfront-porch = <2>;
    			vback-porch = <2>;
    			vsync-len = <10>;
    			hsync-active = <0>;
    			vsync-active = <0>;
    			de-active = <1>;
    			pixelclk-active = <1>;
    		};
    
    		port {
    			lcd_in: endpoint {
    				remote-endpoint = <&dpi_out>;
    			};
    		};
    	};
    };
    
    &am43xx_pinmux {
    
    	matrix_keypad_pins: matrix_keypad_pins {
    		pinctrl-single,pins = <
    			0x24c (PIN_OUTPUT | MUX_MODE7)	/* gpio5_13.gpio5_13 */
    			0x250 (PIN_OUTPUT | MUX_MODE7)	/* spi4_sclk.gpio5_4 */
    			0x254 (PIN_INPUT | MUX_MODE7)	/* spi4_d0.gpio5_5 */
    			0x258 (PIN_INPUT | MUX_MODE7)	/* spi4_d1.gpio5_5 */
    		>;
    	};
    
    	leds_pins: leds_pins {
    		pinctrl-single,pins = <
    			0x228 (PIN_OUTPUT | MUX_MODE7)	/* uart3_rxd.gpio5_2 */
    			0x22c (PIN_OUTPUT | MUX_MODE7)	/* uart3_txd.gpio5_3 */
    			0x230 (PIN_OUTPUT | MUX_MODE7)	/* uart3_ctsn.gpio5_0 */
    			0x234 (PIN_OUTPUT | MUX_MODE7)	/* uart3_rtsn.gpio5_1 */
    		>;
    	};
    
    	i2c0_pins: i2c0_pins {
    		pinctrl-single,pins = <
    			0x188 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)  /* i2c0_sda.i2c0_sda */
    			0x18c (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)  /* i2c0_scl.i2c0_scl */
    		>;
    	};
    
    	i2c1_pins: i2c1_pins {
    		pinctrl-single,pins = <
    			0x15c (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2)  /* spi0_cs0.i2c1_scl */
    			0x158 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE2)  /* spi0_d1.i2c1_sda  */
    		>;
    	};
    
    	mmc1_pins: pinmux_mmc1_pins {
    		pinctrl-single,pins = <
    			0x160 (PIN_INPUT | MUX_MODE7) /* spi0_cs1.gpio0_6 */
    		>;
    	};
    
    	ecap0_pins: backlight_pins {
    		pinctrl-single,pins = <
    			0x164 (PIN_OUTPUT | MUX_MODE0) /* eCAP0_in_PWM0_out.eCAP0_in_PWM0_out */
    		>;
    	};
    
    	edt_ft5306_ts_pins: edt_ft5306_ts_pins {
    		pinctrl-single,pins = <
    			0x74 (PIN_INPUT | MUX_MODE7)	/* gpmc_wpn.gpio0_31 */
    			0x78 (PIN_OUTPUT | MUX_MODE7)	/* gpmc_be1n.gpio1_28 */
    		>;
    	};
    
    	vpfe0_pins_default: vpfe0_pins_default {
    		pinctrl-single,pins = <
    			0x1B0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_hd mode 0*/
    			0x1B4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_vd mode 0*/
    			0x1C0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_pclk mode 0*/
    			0x1C4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data8 mode 0*/
    			0x1C8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data9 mode 0*/
    			0x208 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data0 mode 0*/
    			0x20C (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data1 mode 0*/
    			0x210 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data2 mode 0*/
    			0x214 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data3 mode 0*/
    			0x218 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data4 mode 0*/
    			0x21C (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data5 mode 0*/
    			0x220 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data6 mode 0*/
    			0x224 (PIN_INPUT_PULLUP | MUX_MODE0)  /* cam0_data7 mode 0*/
    			0x1E8 (PIN_INPUT_PULLUP | MUX_MODE7)  /* cam1_data0 mode 0*/
    		>;
    	};
    
    	vpfe0_pins_sleep: vpfe0_pins_sleep {
    		pinctrl-single,pins = <
    			0x1B0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_hd mode 0*/
    			0x1B4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_vd mode 0*/
    			0x1C0 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_pclk mode 0*/
    			0x1C4 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data8 mode 0*/
    			0x1C8 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data9 mode 0*/
    			0x208 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data0 mode 0*/
    			0x20C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data1 mode 0*/
    			0x210 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data2 mode 0*/
    			0x214 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data3 mode 0*/
    			0x218 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data4 mode 0*/
    			0x21C (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data5 mode 0*/
    			0x220 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data6 mode 0*/
    			0x224 (DS0_PULL_UP_DOWN_EN | INPUT_EN | MUX_MODE7)  /* cam0_data7 mode 0*/
    		>;
    	};
    
    	clkout1_pin: pinmux_clkout1_pin {
    		pinctrl-single,pins = <
    			0x270 (PIN_OUTPUT_PULLDOWN | MUX_MODE3)	/* XDMA_EVENT_INTR0/CLKOUT1 */
    		>;
    	};
    
    	cpsw_default: cpsw_default {
    		pinctrl-single,pins = <
    			/* Slave 1 */
    			0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txclk.rmii1_tclk */
    			0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txen.rgmii1_tctl */
    			0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd0.rgmii1_td0 */
    			0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd1.rgmii1_td1 */
    			0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd0.rgmii1_td2 */
    			0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* mii1_txd1.rgmii1_td3 */
    			0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxclk.rmii1_rclk */
    			0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxdv.rgmii1_rctl */
    			0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd0.rgmii1_rd0 */
    			0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd1.rgmii1_rd1 */
    			0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd0.rgmii1_rd2 */
    			0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* mii1_rxd1.rgmii1_rd3 */
    
    			/* Slave 2 */
    			0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a6.rgmii2_tclk */
    			0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a0.rgmii2_tctl */
    			0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a5.rgmii2_td0 */
    			0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a4.rgmii2_td1 */
    			0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a3.rgmii2_td2 */
    			0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a2.rgmii2_td3 */
    			0x5c (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a7.rgmii2_rclk */
    			0x44 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a1.rgmii2_rtcl */
    			0x6c (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a11.rgmii2_rd0 */
    			0x68 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a10.rgmii2_rd1 */
    			0x64 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a9.rgmii2_rd2 */
    			0x60 (PIN_INPUT_PULLDOWN | MUX_MODE2)	/* gpmc_a8.rgmii2_rd3 */
    		>;
    	};
    
    	cpsw_sleep: cpsw_sleep {
    		pinctrl-single,pins = <
    			/* Slave 1 reset value */
    			0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    
    			/* Slave 2 reset value */
    			0x58 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x40 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x54 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x50 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x4c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x48 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x5c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x44 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x6c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x68 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x64 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x60 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    		>;
    	};
    
    	davinci_mdio_default: davinci_mdio_default {
    		pinctrl-single,pins = <
    			/* MDIO */
    			0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)	/* mdio_data.mdio_data */
    			0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0)			/* mdio_clk.mdio_clk */
    		>;
    	};
    
    	davinci_mdio_sleep: davinci_mdio_sleep {
    		pinctrl-single,pins = <
    			/* MDIO reset value */
    			0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
    			0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
    		>;
    	};
    
    	dss_pins: dss_pins {
    		pinctrl-single,pins = <
    			0x020 (PIN_OUTPUT_PULLUP | MUX_MODE1)	/* gpmc ad 8 -> DSS DATA 23 */
    			0x024 (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x028 (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x02c (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x030 (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x034 (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x038 (PIN_OUTPUT_PULLUP | MUX_MODE1)
    			0x03c (PIN_OUTPUT_PULLUP | MUX_MODE1)	/* gpmc ad 15 -> DSS DATA 16 */
    			0x0a0 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS DATA 0 */
    			0x0a4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0a8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0ac (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0b0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0b4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0b8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0bc (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0c0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0c4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0c8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0cc (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0d0 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0d4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0d8 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    			0x0dc (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS DATA 15 */
    			0x0e0 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS VSYNC */
    			0x0e4 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS HSYNC */
    			0x0e8 (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS PCLK */
    			0x0ec (PIN_OUTPUT_PULLUP | MUX_MODE0)	/* DSS AC BIAS EN */
    
    		>;
    	};
    
    	qspi_pins: qspi_pins {
    		pinctrl-single,pins = <
    			0x7c (PIN_OUTPUT_PULLUP | MUX_MODE3)	/* gpmc_csn0.qspi_csn */
    			0x88 (PIN_OUTPUT | MUX_MODE2)		/* gpmc_csn3.qspi_clk */
    			0x90 (PIN_INPUT_PULLUP | MUX_MODE3)	/* gpmc_advn_ale.qspi_d0 */
    			0x94 (PIN_INPUT_PULLUP | MUX_MODE3)	/* gpmc_oen_ren.qspi_d1 */
    			0x98 (PIN_INPUT_PULLUP | MUX_MODE3)	/* gpmc_wen.qspi_d2 */
    			0x9c (PIN_INPUT_PULLUP | MUX_MODE3)	/* gpmc_be0n_cle.qspi_d3 */
    		>;
    	};
    
    	mcasp1_pins: mcasp1_pins {
    		pinctrl-single,pins = <
    			0x10c (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* mii1_crs.mcasp1_aclkx */
    			0x110 (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* mii1_rxerr.mcasp1_fsx */
    			0x108 (PIN_OUTPUT_PULLDOWN | MUX_MODE4)	/* mii1_col.mcasp1_axr2 */
    			0x144 (PIN_INPUT_PULLDOWN | MUX_MODE4)	/* rmii1_ref_clk.mcasp1_axr3 */
    		>;
    	};
    
    	lcd_pins: lcd_pins {
    		pinctrl-single,pins = <
    			0x1c (PIN_OUTPUT_PULLDOWN | MUX_MODE7) /* gpcm_ad7.gpio1_7 */
    		>;
    	};
    
    	usb2_phy1_pins: usb2_phy1_pins {
    		pinctrl-single,pins = <
    			0x2c0 (PIN_OUTPUT_PULLDOWN | MUX_MODE0)
    		>;
    	};
    
    	usb2_phy2_pins: usb2_phy2_pins {
    		pinctrl-single,pins = <
    			0x2c4 (PIN_OUTPUT_PULLUP | MUX_MODE0)
    		>;
    	};
    
    	hardware_pins: hardware_pins {
    		pinctrl-single,pins = <
    			0x000 MUX_MODE7		  /* gpmc_ap0.gpi01_0 */
    			0x150 MUX_MODE3		  /* spi0_sclk.ehrpwm0A */
    			0x1A0 MUX_MODE9		  /* mcasp0_aclkr.gpi0_18 */
    			0x1AC MUX_MODE9		  /* mcasp0_ahclkx.gpi0_3 */
    			0x1A8 MUX_MODE9		  /* mcasp0_axr1.gpi0_2 */
    			0x1A4 MUX_MODE9		  /* mcasp0_fsr.gpi0_19 */
    			0x26C MUX_MODE9		  /* spi2c_cs0.gpi0_23 */
    			0x264 MUX_MODE9		  /* spi2_d0.gpi0_20 */
    			0x268 MUX_MODE9		  /* spi2_d1.gpi0_21 */
    			0x260 MUX_MODE9		  /* spi2_sclk.gpi0_22 */
    		>;
    	};
    };
    
    &i2c0 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&i2c0_pins>;
    	clock-frequency = <100000>;
    
    	tps@24 {
    		compatible = "ti,tps65218";
    		reg = <0x24>;
    		interrupt-parent = <&gic>;
    		interrupts = <GIC_SPI 7 IRQ_TYPE_LEVEL_HIGH>;
    		interrupt-controller;
    		#interrupt-cells = <2>;
    
    		dcdc1: regulator-dcdc1 {
    			compatible = "ti,tps65218-dcdc1";
    			/* VDD_CORE limits min of OPP50 and max of OPP100 */
    			regulator-name = "vdd_core";
    			regulator-min-microvolt = <912000>;
    			regulator-max-microvolt = <1144000>;
    			regulator-boot-on;
    			regulator-always-on;
    		};
    
    		dcdc2: regulator-dcdc2 {
    			compatible = "ti,tps65218-dcdc2";
    			/* VDD_MPU limits min of OPP50 and max of OPP_NITRO */
    			regulator-name = "vdd_mpu";
    			regulator-min-microvolt = <912000>;
    			regulator-max-microvolt = <1378000>;
    			regulator-boot-on;
    			regulator-always-on;
    		};
    
    		dcdc3: regulator-dcdc3 {
    			compatible = "ti,tps65218-dcdc3";
    			regulator-name = "vdds_ddr";
    			regulator-min-microvolt = <1500000>;
    			regulator-max-microvolt = <1500000>;
    			regulator-boot-on;
    			regulator-always-on;
    			regulator-state-mem {
    				regulator-on-in-suspend;
    			};
    			regulator-state-disk {
    				regulator-off-in-suspend;
    			};
    		};
    
    		dcdc4: regulator-dcdc4 {
    			compatible = "ti,tps65218-dcdc4";
    			regulator-name = "v3_3d";
    			regulator-min-microvolt = <3300000>;
    			regulator-max-microvolt = <3300000>;
    			regulator-boot-on;
    			regulator-always-on;
    		};
    
    		dcdc5: regulator-dcdc5 {
    			compatible = "ti,tps65218-dcdc5";
    			regulator-name = "v1_0bat";
    			regulator-min-microvolt = <1000000>;
    			regulator-max-microvolt = <1000000>;
    			regulator-boot-on;
    			regulator-always-on;
    			regulator-state-mem {
    				regulator-on-in-suspend;
    			};
    		};
    
    		dcdc6: regulator-dcdc6 {
    			compatible = "ti,tps65218-dcdc6";
    			regulator-name = "v1_8bat";
    			regulator-min-microvolt = <1800000>;
    			regulator-max-microvolt = <1800000>;
    			regulator-boot-on;
    			regulator-always-on;
    			regulator-state-mem {
    				regulator-on-in-suspend;
    			};
    		};
    
    		ldo1: regulator-ldo1 {
    			compatible = "ti,tps65218-ldo1";
    			regulator-name = "v1_8d";
    			regulator-min-microvolt = <1800000>;
    			regulator-max-microvolt = <1800000>;
    			regulator-boot-on;
    			regulator-always-on;
    		};
    
    	};
    
    	at24@50 {
    		compatible = "at24,24c256";
    		pagesize = <64>;
    		reg = <0x50>;
    	};
    };
    
    &i2c1 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&i2c1_pins>;
    	clock-frequency = <400000>;
    
    	ov2659@30 {
    		compatible = "ti,ov2659";
    		reg = <0x30>;
    		pinctrl-names = "default";
    		pinctrl-0 = <&clkout1_pin>;
    
    		port {
    			ov2659_1: endpoint {
    				remote-endpoint = <&vpfe0_ep>;
    				mclk-frequency = <25000000>;
    			};
    		};
    	};
    
    	edt-ft5306@38 {
    		status = "okay";
    		compatible = "edt,edt-ft5306", "edt,edt-ft5x06";
    		pinctrl-names = "default";
    		pinctrl-0 = <&edt_ft5306_ts_pins>;
    
    		reg = <0x38>;
    		interrupt-parent = <&gpio0>;
    		interrupts = <31 0>;
    
    		reset-gpios = <&gpio1 28 GPIO_ACTIVE_LOW>;
    
    		touchscreen-size-x = <480>;
    		touchscreen-size-y = <272>;
    	};
    
    	tlv320aic3106: tlv320aic3106@1b {
    		#sound-dai-cells = <0>;
    		compatible = "ti,tlv320aic3106";
    		reg = <0x1b>;
    		status = "okay";
    
    		/* Regulators */
    		AVDD-supply = <&dcdc4>;
    		IOVDD-supply = <&dcdc4>;
    		DRVDD-supply = <&dcdc4>;
    		DVDD-supply = <&ldo1>;
    	};
    
    	lis331dlh@18 {
    		compatible = "st,lis331dlh";
    		reg = <0x18>;
    		status = "okay";
    
    		Vdd-supply = <&dcdc4>;
    		Vdd_IO-supply = <&dcdc4>;
    		interrupts-extended = <&gpio1 6 0>, <&gpio2 1 0>;
    	};
    };
    
    &epwmss0 {
    	status = "okay";
    };
    
    &ecap0 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&ecap0_pins>;
    };
    
    &gpio0 {
    	status = "okay";
    };
    
    &gpio1 {
    	status = "okay";
    };
    
    &gpio5 {
    	pinctrl-names = "default";
        	pinctrl-0 = <&hardware_pins>;
    	status = "okay";
    };
    
    &ehrpwm0 {
            status = "okay";
    };
    
    &mmc1 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&mmc1_pins>;
    
    	vmmc-supply = <&dcdc4>;
    	bus-width = <4>;
    	cd-gpios = <&gpio0 6 GPIO_ACTIVE_HIGH>;
    };
    
    &usb2_phy1 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&usb2_phy1_pins>;
    };
    
    &usb1 {
    	dr_mode = "otg";
    	status = "okay";
    };
    
    &usb2_phy2 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&usb2_phy2_pins>;
    };
    
    &usb2 {
    	dr_mode = "host";
    	status = "okay";
    };
    
    &qspi {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&qspi_pins>;
    
    	spi-max-frequency = <48000000>;
    	m25p80@0 {
    		compatible = "mx66l51235l";
    		spi-max-frequency = <48000000>;
    		reg = <0>;
    		spi-cpol;
    		spi-cpha;
    		spi-tx-bus-width = <1>;
    		spi-rx-bus-width = <4>;
    		#address-cells = <1>;
    		#size-cells = <1>;
    
    		/* MTD partition table.
    		 * The ROM checks the first 512KiB
    		 * for a valid file to boot(XIP).
    		 */
    		partition@0 {
    			label = "QSPI.U_BOOT";
    			reg = <0x00000000 0x000080000>;
    		};
    		partition@1 {
    			label = "QSPI.U_BOOT.backup";
    			reg = <0x00080000 0x00080000>;
    		};
    		partition@2 {
    			label = "QSPI.U-BOOT-SPL_OS";
    			reg = <0x00100000 0x00010000>;
    		};
    		partition@3 {
    			label = "QSPI.U_BOOT_ENV";
    			reg = <0x00110000 0x00010000>;
    		};
    		partition@4 {
    			label = "QSPI.U-BOOT-ENV.backup";
    			reg = <0x00120000 0x00010000>;
    		};
    		partition@5 {
    			label = "QSPI.KERNEL";
    			reg = <0x00130000 0x0800000>;
    		};
    		partition@6 {
    			label = "QSPI.FILESYSTEM";
    			reg = <0x00930000 0x36D0000>;
    		};
    	};
    };
    
    &mac {
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&cpsw_default>;
    	pinctrl-1 = <&cpsw_sleep>;
    	dual_emac = <1>;
    	status = "okay";
    };
    
    &davinci_mdio {
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&davinci_mdio_default>;
    	pinctrl-1 = <&davinci_mdio_sleep>;
    	status = "okay";
    };
    
    &cpsw_emac0 {
    	phy_id = <&davinci_mdio>, <4>;
    	phy-mode = "rgmii";
    	dual_emac_res_vlan = <1>;
    };
    
    &cpsw_emac1 {
    	phy_id = <&davinci_mdio>, <5>;
    	phy-mode = "rgmii";
    	dual_emac_res_vlan = <2>;
    };
    
    &elm {
    	status = "okay";
    };
    
    &mcasp1 {
    	#sound-dai-cells = <0>;
    	pinctrl-names = "default";
    	pinctrl-0 = <&mcasp1_pins>;
    
    	status = "okay";
    
    	op-mode = <0>;
    	tdm-slots = <2>;
    	serial-dir = <
    		0 0 1 2
    	>;
    
    	tx-num-evt = <1>;
    	rx-num-evt = <1>;
    };
    
    &dss {
    	status = "okay";
    
    	pinctrl-names = "default";
    	pinctrl-0 = <&dss_pins>;
    
    	port {
    		dpi_out: endpoint@0 {
    			remote-endpoint = <&lcd_in>;
    			data-lines = <24>;
    		};
    	};
    };
    
    &rtc {
    	status = "okay";
    };
    
    &wdt {
    	status = "okay";
    };
    
    &cpu {
    	cpu0-supply = <&dcdc2>;
    };
    
    &vpfe0 {
    	status = "okay";
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&vpfe0_pins_default>;
    	pinctrl-1 = <&vpfe0_pins_sleep>;
    
    	/* Camera port */
    	port {
    		vpfe0_ep: endpoint {
    			remote-endpoint = <&ov2659_1>;
    			if_type = <2>;
    			bus_width = <8>;
    			hdpol = <0>;
    			vdpol = <0>;
    		};
    	};
    };
    
    &wkup_m3 {
    	ti,scale-data-fw = "am43x-evm-scale-data.bin";
    };

    I think that this isn't the right way to configure this, but it worked. I just defined the pins inside &am43xx_pinmux, and then at the end i set those pins configuration with this:

    &gpio5 {
    	pinctrl-names = "default";
        	pinctrl-0 = <&hardware_pins>;
    	status = "okay";
    };

    How is the right way to do it?

    thanks,

    Pedro

  • Hi Pedro,

    If your goal is to control these pins (toggle their output) with GPIO sysfs entry, then the above approach should be OK.

    Best Regards,
    Yordan