Hi,
I am using MP3DEC 1.31.001 on DM6446 with DVSDK 2.00.00.22 with MVL5. My pipeline runs well for 12+ hours, actually everytime around 12:27m, then it stops. Seems like the mp3dec has a limit number of output counts. I do have "watermark = false" and did not hear the "watermark" beep at all. But I am not sure if there is anything else I need to pay attention to. Thanks all for help~~~