Other Parts Discussed in Thread: TMS320DM6437
Hi,
I'm running the "Accessing pixels in a frame on DM643x" (http://processors.wiki.ti.com/index.php/Accessing_pixels_in_a_frame_on_DM643x) example code in CCS v4.1.2.00027, using the TMS320DM6437 evaluation board.
So far, I've been able to run the project, but I'd like to view the frames in image analyzer.
From the source code I see the frames are720x480 16-bit YCbCr422 images.
Can someone share the complete image settings (pixel stride, mask, etc)?
Thank you