Hi Guys,
We are using Spansion 8-bit NAND, we were able to detect NAND info.
i have followed above document for
Flashing 1st stage to NAND from 2nd stage in SD boot & Flashing 2nd stage to NAND from 2nd stage in SD boot
as we are booting from sd card.
we are able to write.
Now we want to copy uImage and filesystem in to NAND. how to do it?
Logs in case:
DRAM: 1 GiB
NAND:
nand_init_chip -> NAND base_addr-> 8000000
Searching for NAND device @ GPMC CS:0
board_nand_init : NAND is 8-bit
HW ECC BCH8 Selected
DM385 -> Busw: 0
DM385 : GPMC -> 810 CONTROL_STATUS -> 317
nand_get_flash_type: READ ID 01,f1 against 01,f1
128 MiB
MMC: : 0, ON-BOARD SDIO: 1
Net: cpsw
0
DM385_IPNC#fatls mmc 0
83296 mlo
211016 u-boot.bin
2637408 uimage
108460 u-boot.min.nand
211192 u-boot_nand.bin
5 file(s), 0 dir(s)
thanks & regards,
Ganesh