Hi,
i build the ti sdk package for am437x-evm using following link (on ubuntu )
i have .ipk packages under --tisdk/build/arago-tmp-external-linaro-toolchain/deploy/ipk/am437x_evm/ , i want build in the filesystem to use. i was using following command but got error
dpkg install [package_ipk].ipk
also tried with dpkg install [package_ipk].ipk command but it not work
Error:
dpkg: warning: parsing file '/var/lib/dpkg/available' near line 17730 package 'libopencv-aruco3.1':
'am437x_evm' is not a valid architecture name: character `_' not allowed (only letters, digits and characters `-')
dpkg: warning: parsing file '/var/lib/dpkg/tmp.ci/control' near line 9 package 'libopencv-aruco3.1':
'am437x_evm' is not a valid architecture name: character `_' not allowed (only letters, digits and characters `-')
dpkg: error processing archive libopencv-aruco3.1_3.1+git0+f7f004f623-r0.tisdk5_am437x_evm.ipk (--install):
package architecture (am437x_evm) does not match system (amd64)
Errors were encountered while processing:
libopencv-aruco3.1_3.1+git0+f7f004f623-r0.tisdk5_am437x_evm.ipk
please tell me how to build .ipk packages and how to use it??