Other Parts Discussed in Thread: AM3357, SYSBIOS
Hi team,
A customer is looking into designing in the AM3357 and has a few questions about the peripherals and supported functions.
Thanks in advance!
Billy
----
-Is BOOTP/DHCP supported?
-Is RSTP supported on chip or do we have to implement in our software?
-For Ethernet/IP: How many explicit and IO connections are supported in the stack? and what types of connections? i.e. Exclusive owner, Input only, Listen Only? Can we add our own vendor specific objects and also add more ODVA objects such as the energy objects?
-For Modbus TCP: What function codes are supported? and for the ones that are not supported can we add them in our software as well and add vendor specific function codes?
-For Profinet: Is the Profidrive profile available in the stack? Does is support MRP?
-How easy is it for us to integrate our webpage into the design if we use this chip?
-Who is the third party that owns the Ethernet/IP and Profinet stacks and what is an estimate for licensing cost?