Other Parts Discussed in Thread: AM3358
Hi,
I have the following GPMC configuration on a AM3358 device to NOR FLASH (Spansion S29GL101GP):
- NOR Flash attached to CS0 of GPMC with NON multiplexed address and data bus
- NOR flash is mapped to address 0x10000000 ( 16MB)
following is the code:
base_addr = 0x10000000;
/* Auto Select Entry */
*((unsigned short *)base_addr + 0x555) = 0x00AA; /* write unlock cycle 1 */
*((unsigned short *)base_addr + 0x2AA) = 0x0055; /* write unlock cycle 2 */
*((unsigned short *)base_addr + 0x555) = 0x0090; /* write autoselect command */
//Read Manufacturer Id
manuf_id = *((unsigned short *)base_addr + 0x00); /* read manuf. id */
//Read Device Id
Dev_id_1 = *((unsigned short *)base_addr + 0x001); /* read Dev. id */
//Read Device Id
Dev_id_2 = *((unsigned short *)base_addr + 0xE); /* read Dev. id */
This code does put the NOR Flash into "AutoSelect" mode and reads manufacturer code, device code and block protection status of first block.
The code works fine if I step over the code in CCS and the signals on the scope look as they should.
But I could able to read Manufacturer Id 0x01, but Dev ID reading as 0xFFFF instead 0x227E.
I have changed GPMC configuration to NOR FLASH type,16 bit bus width with reference of NAND read write code . Following is the configuration of GPMC. Let me know any other configuration need to change.
GPMC_A1 to GPMC_A26 address lines and GPMC_DQ0 to GPMC_DQ15 data lines used.
/*****************************************************************************/
/*
** Macros which defines the NAND timing info.
**
*/
#define NAND_CSWROFFTIME (30)
#define NAND_CSRDOFFTIME (31)
#define NAND_CSONTIME (0)
#define NAND_ADVONTIME (0)
#define NAND_ADVAADMUXONTIME (0)
#define NAND_ADVRDOFFTIME (31)
#define NAND_ADVWROFFTIME (31)
#define NAND_ADVAADMUXRDOFFTIME (0)
#define NAND_ADVAADMUXWROFFTIME (0)
#define NAND_WEOFFTIME (31)
#define NAND_WEONTIME (3)
#define NAND_OEAADMUXOFFTIME (31)
#define NAND_OEOFFTIME (31)
#define NAND_OEAADMUXONTIME (3)
#define NAND_OEONTIME (1)
#define NAND_RDCYCLETIME (31)
#define NAND_WRCYCLETIME (31)
#define NAND_RDACCESSTIME (28)
#define NAND_PAGEBURSTACCESSTIME (0)
#define NAND_BUSTURNAROUND (0)
#define NAND_CYCLE2CYCLEDIFFCSEN (0)
#define NAND_CYCLE2CYCLESAMECSEN (1)
#define NAND_CYCLE2CYCLEDELAY (0)
#define NAND_WRDATAONADMUXBUS (15)
#define NAND_WRACCESSTIME (22)
int GPMC_NOR_CONFIG()
{
volatile unsigned int conf = 0;
volatile unsigned int i = 0;
volatile unsigned short int p_read[20000];// = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};
GPMCClkConfig();
GPMCModuleSoftReset(SOC_GPMC_0_REGS);
while (GPMCModuleResetStatusGet(SOC_GPMC_0_REGS) != 1);
GPMCIdleModeSelect(SOC_GPMC_0_REGS, GPMC_IDLEMODE_NOIDLE);
GPMCCSConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_CS_DISABLE); // Chip Select should be disabled when the GPMC configuration is being done..
/* Disable all interrupts */
GPMCIntDisable(SOC_GPMC_0_REGS, GPMC_FIFOEVENT_INT);
GPMCIntDisable(SOC_GPMC_0_REGS, GPMC_TERMINALCOUNT_INT);
GPMCIntDisable(SOC_GPMC_0_REGS, GPMC_WAIT0EDGEDETECTION_INT);
GPMCIntDisable(SOC_GPMC_0_REGS, GPMC_WAIT1EDGEDETECTION_INT);
/* Timeout control disable */
GPMCTimeOutFeatureConfig(SOC_GPMC_0_REGS, GPMC_TIMEOUTFEATURE_DISABLE);
GPMCWaitPinSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_WAIT_PIN0);
GPMCWaitPinPolaritySelect(SOC_GPMC_0_REGS, GPMC_WAIT_PIN0,GPMC_WAIT_PIN_POLARITY_LOW);
GPMCWriteProtectPinLevelCtrl(SOC_GPMC_0_REGS, GPMC_WP_PIN_LEVEL_HIGH);
//GPMCWriteProtectPinLevelCtrl(SOC_GPMC_0_REGS, GPMC_FORCEPOSTEDWRITE_ENABLE);//GPMC_FORCEPOSTEDWRITE_ENABLE
//configuration as per Table 7-27 of TRM [NOR Memory Type]
GPMCDevTypeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_DEVICETYPE_NORLIKE); // NOR type Device selected on GPMC.
GPMCDevSizeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_DEVICESIZE_16BITS); // 16 bit NOR device selected.
GPMCAddrDataMuxProtocolSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_MUXADDDATA_NOMUX ); // Address Data NON Multiplexing
// GPMCDevPageLenSet(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0,GPMC_DEV_PAGELENGTH_FOUR); // ****This should not be effective as the page length will be supported in synchronous mode
//GPMCSyncWrapBurstConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0,GPMC_WRAPBURST_DISABLE); // We are not using syncronous mode so this statement is not effective
GPMCTimeParaGranularitySelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_TIMEPARAGRANULARITY_X2); //GPMC_TIMEPARAGRANULARITY_X1// support for slower devices
GPMCFclkDividerSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0,GPMC_FCLK_DIV_BY_4); // GPMC_CLK :- clock division by 4 i.e. 100MHZ /4 = 25MHZ TODO:- Need to confirm on this
// GPMCClkActivationTimeConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0,GPMC_CLKACTIVATIONTIME_ATSTART ); // Not needed in our case, is valid for synchronous read write
GPMCAccessTypeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_MODE_READ, GPMC_ACCESSTYPE_SINGLE); // single read access
GPMCReadTypeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_READTYPE_ASYNC); // read type asynchronous
GPMCAccessTypeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_MODE_WRITE, GPMC_ACCESSTYPE_SINGLE); // single write access
GPMCWriteTypeSelect(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_WRITETYPE_ASYNC); // write type asynchornous
//configuration as per Table 7-28 of TRM [NOR Chip Select Configuration]
//GPMCBaseAddrSet(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, 0x10); // A29:A24 = 010000
//GPMCMaskAddrSet(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_CS_SIZE_16MB); //16MB
GPMCBaseAddrSet(SOC_GPMC_0_REGS, 0, 0x10000000 >> 24);
GPMCMaskAddrSet(SOC_GPMC_0_REGS, 0, GPMC_CS_SIZE_16MB);
// NOR Timing Configuration has to be completed on 10/08/2015 by Mohit Hada
// CS# de-assertion time from start cycle time for write accesses - NAND_CSWROFFTIME
// CS# de-assertion time from start cycle time for read accesses - NAND_CSRDOFFTIME
// CS# assertion time from start cycle time - NAND_CSONTIME
// No extra delay added.
// Check section 7.1.3.3.9.2 of TRM for details on this
conf = GPMC_CS_TIMING_CONFIG(NAND_CSWROFFTIME,
NAND_CSRDOFFTIME,
0,
NAND_CSONTIME);
GPMCCSTimingConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, conf);
// ADV# de-assertion time from start cycle time for write accesses - NAND_ADVWROFFTIME
// ADV# de-assertion time from start cycle time for read accesses - NAND_ADVRDOFFTIME
// ADV# assertion for first address phase when using the AADMultiplexed protocol - NAND_ADVONTIME
// Check section 7.1.3.3.9.3 of TRM for details on this
conf = GPMC_ADV_TIMING_CONFIG(NAND_ADVAADMUXWROFFTIME,
NAND_ADVAADMUXRDOFFTIME,
NAND_ADVWROFFTIME,
NAND_ADVRDOFFTIME,
0,
NAND_ADVAADMUXONTIME,
NAND_ADVONTIME);
GPMCADVTimingConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, conf);
// TODO:- Will check this?
conf = GPMC_WE_OE_TIMING_CONFIG(NAND_WEOFFTIME,
0,
NAND_WEONTIME,
NAND_OEAADMUXOFFTIME,
NAND_OEOFFTIME,
0,
NAND_OEAADMUXONTIME,
NAND_OEONTIME);
GPMCWEAndOETimingConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, conf);
conf = GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(NAND_RDCYCLETIME,
NAND_WRCYCLETIME,
NAND_RDACCESSTIME,
NAND_PAGEBURSTACCESSTIME);
GPMCRdAccessAndCycleTimeTimingConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, conf);
// TODO:- Will check this?
conf = GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(
NAND_CYCLE2CYCLEDELAY,
NAND_CYCLE2CYCLESAMECSEN,
NAND_CYCLE2CYCLEDIFFCSEN,
NAND_BUSTURNAROUND
);
GPMCycle2CycleAndTurnArndTimeTimingConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, conf);
GPMCWrAccessAndWrDataOnADMUXBusTimingConfig(SOC_GPMC_0_REGS,
GPMC_CHIP_SELECT_0,
NAND_WRACCESSTIME,
NAND_WRDATAONADMUXBUS);
GPMCCSConfig(SOC_GPMC_0_REGS, GPMC_CHIP_SELECT_0, GPMC_CS_ENABLE); // Chip Select should be enabled after the GPMC configuration is done..
return 0;
}
Thanks & Regards,
Sudheer A.