This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Boot sends no sequence on serial port.

If I understand correctly I should see some sequence of bytes from the serial port when the DM365 is reset or powered up.  I switched both BTSEL3 and BTSEL2 (pos 1 and pos 2) on.  The manual for the EVM mangles the labeling and logic of these switched beyong belief!!!  But the sfh_DM36x.exe program hangs waiting for the DM365.

I also see nothing on the serial port if I use CuteCom.  Just for confirmation this is what my switch 4 looks like.  I haven't changed anything else.  I'm assuming it's 115200/8/N/1 no flow control.

          B

          T

          S

          E

          L

          3

SW4 - UP UP DOWN DOWN DOWN DOWN

  • John,

    Here are some details:

    BTSEL[2:0] = 011 = UART Boot  (datasheet section 3.2.1)

    UART Boot SW4-pin setting [1-2-3-4-5-6] = off-on-on-off-off-off 

    '115200/8/N/1 no flow control' is correct.

    FYI; silicon revision 1.1, the UART Boot is sort of broken, silicon rev 1.2 is fixed. (see errata)

    Let me know if this resolves your issues.

    regards,

    miguel

     

     

  • Miguel,

    Correction in my switch illustration.  BTSEL3 should be BTSEL2.

    According to the EVMDM365 tech reference manual the switch setting is....

    UART Boot SW4-pin setting [1-2-3-4-5-6] = on-on-off-off-off-off  (1.5 Boot / Configuration Switch Settings)

    Since pos 1 (leftmost) is designated BTSEL2, this conflicts with the data sheet as you noted....

    BTSEL[2:0] = 011 = UART Boot  (datasheet section 3.2.1)

    So I tried both and got no results either way.  My board is "REV C" and the marking on the chip is....

    TMX320

    DM365AZCE

    YFA-8CA2FEW

    EL

    Could this be a revision 1.1 chip?

  • New information now.  I thought it wasn't working with the BTSEL you suggested from the data sheet but apparently it was.

    The sfh_DM36x.exe application was just "waiting for DM365', but when I went back and checked with CuteCom I was seeing a sequence come out on the serial port.

    What has me wondering is that sfh_DM36x.exe says that it's using /dev/ttyS0, but while it's waiting I can go to CuteCom and open the same device and get a sequence.  If sfh_DM36x.exe had acually opened /dev/ttyS0 I would think that CuteCom would have failed to open it.

    My code sequence is.

    P, 0xf4, t, I, G, 0x09, 0xf8

    Well at least I know the board is doing something.

    John

  • This doesn't look good.  sft_DM36x.exe is seeing the port.  I used the verbose option and it started dumping the erroneous sequence that's being sent.  After reviewing the source code for sfh_DM36x.exe it appears the code sequence should be...

    B, O, O, T, M, E

    and not....

    P, 0xf4, t, I, G, 0x09, 0xf8

    The serial port works fine when running normally.  Could this be the revision 1.1 problem?  Can it be fixed?

    John

  • John,

    DM365AZCE indicates that is Revision 1.1 (as noted in the errata device symbolization)

    Unfortunately this cannot be fixed as it is a Rom bootloader problem, it is fully  fixed in 1.2.

    There is a workaround noted in the errata, not sure how to implement it though..

    fixed the msg..

    Excerpt from errata:

    details of issue are:

    The OSM_SEL (Over-Sampling Mode Select) bit in the UART0 MDR (Mode Definition

    Register) should be set to 0. The current boot ROM code sets it to 1.

    OSM_SEL = 0: 16x over sampling => Divisor value = clk/(16*baud_rate)

    OSM_SEL = 1: 13x over sampling=> Divisor value = clk/(13*baud_rate)

    The choice of divisor value for UART is affected by OSM_SEL for a particular baud_rate.

    workaround:

    To workaround this issue, use higher baud rate code. The desired baud rate of 115200

    should be increased to 16/13 times (i.e., ~141800).

    regards,

    miguel

     

  • I think we are just going to order a later revision chip and have the existing one replaced at this time.

  • John,

    Sounds good, sorry for the inconvenience.

    regards,

    miguel