Hi,
I have read through the various posts and understand I need to run (from Windows) the following command...
sfh_DM35x.exe -nandflash <UBL binary file> <binary application file>
However I do not have a binary of u-boot for the DM355. I have a UBL binary file, just no U-Boot for the DM355.
Can anyone point me to where I can download it? I only have a Winodws machine so I cannot unwrap(or install) the PSP.