I'm running PSDKLA 3.01 on Vayu ES 2.0, Rev H EVM.
I need to connect and external HDMI touchscreen display. When I connect the display to the HDMI connector along with the USB input for touch, the external display only shows the weston background, but not the Matrix GUI.
The display in question is Lilliput HDMI multi touch display:
What should I do so that the external display shows Matrix GUI and touch works? In other words, I want to make the external HDMI display my default touch screen display.
Thanks,
Kaushal