This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZdsp5535 not found in CCS6

Hello guys, 

I used CCS4 and I used target configurations and so, I run the LEDs and LCD examples successfully, but when I installed CCS6, I cannot create the target configurations since EZDSP5535 doesn't exist anymore, also “Texas Instruments XDS100v2 USB Emulator” doesn't exist anymore, now it has a very similar name but it says "probe" I am assuming it's the same.

Could you please help to solve this EZDSP5535 missing issue?

Thanks,

CArlos

  • Carlos,

    It seems that you did not choose the C5000 device family during the installation wizard for CCSv6. You can go back and -re-run the same installer at the installation location, but this time choose the C55x device family.

    In my machine with CCSv6, the target config connection is named "Texas Instruments XDS100v2 USB Debug Probe".

    Lali