This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Method of SRIO communication using two C6670EVM

Guru 15520 points

Hi,

I have a question about AMC connector of C6670EVM.
My customer are planning to use 2 C6670EVM and want to check SRIO communication between these two EVM.
They want to know the method of realizing 2EVM SRIO communication.

They are planning to get following chassis platforms(MicroTCA-blu!eco) from ELMA:
www.elma.com/.../

If anyone knows please give me answers against following questions:
Q1.Is it available to connect two C6670EVM to above chassis platforms via AMC connector of C6670EVM?
Q2.If Q1 answer is yes, is it available to communicate two C6670EVM via SRIO?
   They are worrying about the communication environment whether there is any problem or not.

By the way, I already introduced CI Dual EVM Breakout card which can connect two C6670EVM
and realize SRIO communication.

best regards,
g.f.