Other Parts Discussed in Thread: TMS320C6678
Hi all,
I'm trying to use The Multicore Navigator (QMSS and CPPI) on a C6678 DSP using the new SDK (v 03.01.00.06).
I started using the pdk_C6678_1_1_2_6 examples (the only available, if my info are correct) and tried to use them with the new version with the aid of the migration guide.
The problem is that libraries are changed and a lot of defines are not in their place (this is the problem found so far).
I was wondering if anybody has already done a similar migration because the migration guide doesn't tell where those defines have been moved.
Simpliest solution of course is to copy paste the defines in another .h file, but you understand it is a lot of work and it isn't a certain solution.
Any help would be very much appreciated.
PS: please find below some specifications:
DSP: TMS320C6678;
Evaluation board: TMSEVM6678LE;
CCS Version: 6.2.0.00050;
Compiler Version: v8.1.2.
SDK version: v 03.01.00.06
PDK version: v 2.0.3
Bios version: v 6.46.2.47
IPC version: v 3.43.2.04