Other Parts Discussed in Thread: OMAP-L138, TMS320C6748
Hi,
In my desing i am using 2 codecs (tlv320aic3106). As a configuration port I'm using SPI instead of the I2C port (used on the C6748 SOM module).
unfortunately I didn't realise the amount of effort that I will need to bring SPI to work...
It will be very helpfull if anybody had a skeletton or code example for configuring an SPI port?
The configuration I need is something like :
-master mode
- no Dma
-4-Pin Option with /SPIx_SCS[n]
- Clock : 400KHz or something like that
Thank's for your help
Bruno