Other Parts Discussed in Thread: TMS320C6748
Hello this is the first time to use a TMS320C6784. Thanks for being patient. I am not finding some of the information I need.
1) I plan to boot in the Direct NOR Boot mode. I do not see any information on how the determines whether the external flash is 1.8 or 3.3V. Can you give me a reference for this?
2) I was planning to configure the BOOT pins for NOR FLASH boot mode only. However I see that there is an emulator debug boot mode. I am not sure why this would be used? Do I need it when I am running with the emulator for debug mode?
Thanks for any help,
GG