This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error connectin target

i need one help. c5505 Board assembling is over sir. i checked power supply and all. power supply is working fine, and i checked on board Emulator sir.By using Mprog i have loaded Texas serial number (XDS100 EMU). It is also working properly sir. But i have faced problem When i connect the device. when i connect the kit C5505 to EMU (on board) the target was not connected sir. This is the error i got it sir. Error connecting to the target: Error 0x80002240/-121 Fatal Error during: Initialization, OCS, Control, i dont know what is the problem. am using CCS 4. i think i didnt configure correctly in Software side. This is the first time am using CCS 4. kindly help for this time sir.