This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x UART use leads to high CPU load

Other Parts Discussed in Thread: TL16C554, AM3352

Dear Champion, 

  Today I received one issue related with the AM3352 UART usage. The OS is Linux SDK 7.0. Customer use 4 UART ports in their design. In addition, they also used the TL16C554 to extend 4 UART by the GPMC port. 

  But they found that the CPU loading is very high when 4 UART port worked at the same time. Each would take 20~30% when using the TOP command. However, there's no issue with the GPMC extended UART ports, < 10%.

  As I see some discussion here, I would like to know whether changing this driver could help to low down the CPU loading? Is there any similar case in your side to solve this issue?