I am currently using CCSv4's Platinum Trial Version. I used to be able to connect to the OMAPL138 on both the ARM side and the DSP side. Now when I try to connect to the ARM side I get the following error:
"The GEL callback "OnTargetConnect()" for the target "Spectrum Digital XDS510USB Emulator_0/ARM9_0" is still processing.
The function could contain an infinite loop.
Do you wish to pause the processing of this function and continue?"
Connecting to the DSP side gives me no errors. I've seen other posts on the forum but none seem to answer my question. I've tried to restart the board and my PC but none of this seemed to recover the ARM side. When I put print statements into the GEL file it appears to be getting hung up on the very first peripheral power on.
I have also tried to use a different SOM on a different evaluation board but that did not resolve the issue. This could possibly mean that it may be a CCS4 specific issue. How can I connect to the ARM side of the DSP again using CCS4?
GEL output:
"
ARM9_0: Output: Memory Map Cleared. ARM9_0: Output: --------------------------------------------- ARM9_0: Output: Memory Map Setup Complete. ARM9_0: Output: --------------------------------------------- ARM9_0: Output: Enabling Full EVM PSCs... ARM9_0: The GEL callback "OnTargetConnect()" is no longer running atomically "