We would like to set up a C6457 on a board that allows us to boot from either the FLASH connected to the EMIF, or Ethernet. Based on how we connect our system to the outside world, we will want to have either method available at all times. Is there a way to configure the DSP that allows us to boot from either method any time we want? How do we tie mode pins, set up or interfaces, etc to allow this flexibility?
Also, related, on a new board that has never been powered-up before, how do you suggest we boot the DSP, get our program into the FLASH? We would like to use blank FLASH on the board, and at first time power-up, run a bootloader/FLASHprogramming utility to bring data into the DSP via ethernet, then use it to program the FLASH via EMIF. Can this be done? What are your recommendations.
Thank you,
Bryan Busacco.