Other Parts Discussed in Thread: TMS320C6747
Hello,
I am designing a board with a TMS320C6747 and I have the following question related to USB (I am using only USB0):
The DSP will be always in slave mode.
1. How to connect the VBUS pin? Pull-up to the local 5.1V?
2. How to connect the 5V from the connector?
3. Can I connect the Ground from the connector to my local ground on the board?
4. Do I need to use 33R resistors on the lines DM DP?
5. Can I leave DRVVBUS unconnected?
Thank you in advance, any other recommandation is welcome.
Oliivier