This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Active Noise cancellation System - Requirement/Queries

Hi,

Please find our requirement/Queries below for the Active Noise Cancellation DSP:

1) It should support at least 2 MIC(Analog & Digital) and 1 Speaker (Approximately 1W to 3W) which works simultaneously.

2) Expecting the DSP to be programmable such that we can have in house developed algorithm ported.

3) Our final application is a real time system and therefore we are expecting very minimal delay between input/output (excluding the algorithm delay)

4) Expecting EVK to be available for the DSP which includes CCS, debugging tool

5) Expecting the audio sampling rate to be in the range from 8KHZ to 48KHZ and channels from mono to stereo.

6) Will the DSP support double precision algorithm directly or do we have to restricted to float operations

7) How is scheduling for input and output done on the DSP for real time applications.

Thanks for your support and hoping to receive a reply from you soon.

Regards,

Venkadesan.