Hi all:
I want to build ubl in linux system. And the source of ubl have file of "makefile". Input command "make", it's has error
"timake: Commond not found".
I want to know whether it build UBL in linux? if it can, how to build?
Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all:
I want to build ubl in linux system. And the source of ubl have file of "makefile". Input command "make", it's has error
"timake: Commond not found".
I want to know whether it build UBL in linux? if it can, how to build?
Thanks a lot!
Hi,
"timake" is the make utility that comes along with the TI CCS tool chain. LSP 2.10 and LSP 3.10 for DM365 currently use only TI CCS tool chain for UBL compilation. I have sent your request to the LSP development team for any further pointers on your request and they would get back to you with more details.
Regards,
Anshuman
PS: Please mark this post as verified, if you think it has answered your question. Thanks.
Hi Anshuman,
I also had same problem(UBL linux build).. do we have any solution for it??
I am new to TI platform and trying to port DVSDK 3.10 to IPNC(DVSDK 2.10) for DM365.
I started by flashing pre-build(for DVSDK 3.10) ubl and u-boot for EVM to IPNC, but camera didnt boot(no massage in serial consol) so, I guess I need to modify UBL code to match IPNC board.
It would be great help if you can provide me some guidance for porting DVSDK3.0 to IPNC.
Kind Regards,
Alex
Hi,
Has any development been made in being able to recompile and rebuild the UBL that is included with DVSDK4, in linux without CCS?
I'm using dvsdk_4_00_00_22, modded UBL to set the clocks and DDR2 parameters for using a DM368, and IIRC I just typed.... "make ubl" from the dvsdk base directory.
John A