This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: TI-RTOS "System Overview" apparently not working under new CCSv7 install

Part Number: CC1310

Tool/software: Code Composer Studio

Hi folks-

After installing CCSv7, with a previous install of TI-RTOS 2.21 for CC13xx/26xx on my system (which the CCSv7 installer appears to have detected), I tried creating a new CC1310F128 project.  When I open the TI-RTOS config file for editing, in the GUI configurator ("TI-RTOS" tab as opposed to "cfg Script" tab), the "System Overview" button does not work.  You can click it but it goes nowhere.  In CCSv6.2 I would see a graphical view of the TI-RTOS components and could click to import/enable or configure them as necessary.

Example video demonstrating this: https://youtu.be/4QNjHRt49ls

(Note that Microsoft Game DVR seems to show the mouse cursor a tad higher than it actually was, so it looks like I'm clicking above the link when in fact I was clicking on the link... strange bug in the video recorder)