Hi
Does data pins of I2S(data in & out) must configure to AXR0 and AXR1 with McAsp1 port ?
Can I configure AXR5 & AXR6 as data pin in I2S mode and AXR0~AXR1 for I2C use?
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Does data pins of I2S(data in & out) must configure to AXR0 and AXR1 with McAsp1 port ?
Can I configure AXR5 & AXR6 as data pin in I2S mode and AXR0~AXR1 for I2C use?
thank you.
Hi Mickey,Each McASP's data pin (AXR1-16) can be configured absolutely independently as Rx or Tx.
Mickey,
Correct, MCASP has independent serializers/deserializrers on each data pin. You can enable/disable as Rx/Tx according to your application.
Yo can even pass different data formats through the different serializers.
Regards,
Stan