This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: TRM typo

Part Number: AM4378

Hi,

I have simple question.

According to AM437x Datasheet ( SPRUHL7F–April 2014–Revised September 2016 ) Table 9-171. EMF4D_SDRAM_CONFIG Regiser Field Description,

EBANK filed :

External chip select setup.
Defines whether SDRAM accesses will use 1 or 2 chip select lines.
Set to 0 to use pad_cs_o_n[0] only.
Set to 1 to use pad_cs_o_n
[1:0].
This bit will automaticlly be set to 0 if reg_cs1nvmen field in the
LPDDR2 NVM is set to 1.


I think red coloer part is typo.  Collect is the below.

This bit will alutomatically be set to 0  if CS1NVMEM filed in the LPDDR2 NBM is set to 0".

How do you think about this?

Best regards,

Michi