I'm attempting to create a project for the C66x DSP core on the AM5716 processor. The SDK release notes recommend using version 8.1.x of the compiler, however the project I'm creating has a shared build procedure, source files, and other resources with a project using the 7.4.x compiler. I was wondering if this is a hard and fast requirement or if this older version of the compiler will work?