Tool/software: TI-RTOS
Hi,
We are currently investigating using the Sitara AM5726 in one of our products. Right now, I am testing different audio codecs performance on the DSP. The ARM (which is running Linux) is sending encode/decode request to the DSP cores using IPC MessageQ. The ARM allocates a CMEM shared region that is used by both the ARM and the DSP to share the audio data (encoded or PCM).
Now, that CMEM region is currently in DDR. I would like to put that CMEM region in the L3 shared memory (OCMC).
I see in the am57xx-evm-cmem.dtsi that we do have a CMEM block region in OCMC3 :
/ {
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
cmem_block_mem_0: cmem_block_mem@a0000000 {
reg = <0x0 0xa0000000 0x0 0x0c000000>;
no-map;
status = "okay";
};
cmem_block_mem_1_ocmc3: cmem_block_mem@40500000 {
reg = <0x0 0x40500000 0x0 0x100000>;
no-map;
status = "okay";
};
};
cmem {
compatible = "ti,cmem";
#address-cells = <1>;
#size-cells = <0>;
#pool-size-cells = <2>;
status = "okay";
cmem_block_0: cmem_block@0 {
reg = <0>;
memory-region = <&cmem_block_mem_0>;
cmem-buf-pools = <1 0x0 0x0c000000>;
};
cmem_block_1: cmem_block@1 {
reg = <1>;
memory-region = <&cmem_block_mem_1_ocmc3>;
};
};
However, I can't seem to allocate in CMEM block 1.
Can this be done? Or is this block already in use by another part in the system?
Regards,
- David