Other Parts Discussed in Thread: OMAP3530
Hey, experts
QUESTION 1:
When I take a look of the following file regarding to Code engine
./ti-codec-h264-dec/omap3530_h264dec_2_01_007_production/packages/ti/sdo/codecs/h264dec/app/Client/Test/Src/TestAppDecoder.c
in Line 788:
retVal = ividDecFxns->process((IVIDDEC2_Handle)handle,
(XDM1_BufDesc *)&inputBufDesc,
(XDM_BufDesc *)&outputBufDesc,
(IVIDDEC2_InArgs *)&inArgs.viddecInArgs,
(IVIDDEC2_OutArgs *)&outArgs);
I can not find where the "process" function has been defined. How the H.264 decoder will go through with this?
is that "This sample test application does not depict the actual function parameter or control code. It shows the basic flow of the code."
2. QUESTION 2:
Where can i put the reference code from JM, like "ldecode.c" and so on? i mean which directory?
Thank you for any body giving hints on.
All bests,
davie