Part Number: TMDSEVM6657
Other Parts Discussed in Thread: SYSBIOS
Hi experts,
we have a little problem with auto-negatioation, we have used as design base
NIMU helloword demo ad it's running without any problem in both directions.
When we remove the cable RJ45 the application is not able to send
anymore packets, but it's able to receive all the packets.
We don't know if it's a real auto-negotiation problem or not.
Another problem that we have seen (we think it's the same) if the board start
without any connection the Task remains in pending till the eth connection
arriving. But in this case no sent packets are possible.
Our SW used on Linux host machine:
*) Code Composer 6.1.3.00034 (CCS6.1.3.00034_linux.tar.gz)
*) SDK 3.0.0.4 (ti-processor-sdk-rtos-c665x-evm-03.00.00.04-Linux-x86-Install.bin)
*) SYSBIOS 6.46.0.23 (bios_setuplinux_6_46_00_23.bin for posix porting)
*) pdk_c665x_2_0_2
*) ndk_2_24_03_35
Regards,
Dario