This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Flashing images to emmc in uart boot mode +am335x

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hi All,

We are using ti-processor-sdk-3.00.00.04+am335x evm equal custom board.Kernel version is 4.4.12(1.7MB),u-boot-2016-05(~400kb) and rootfs size is 80MB.we want to flash images to emmc from uart booting is it possible?

we loaded u-boot and kernel images into RAM.But how to load file system from uart booting?

Any body tried this can guide me.Because in our case emmc and sd interfaces connected to same interface.So unable to load images through sd booting. Ethernet is not available .ie reason we are trying to flash images to emmc from uart booting.

Thanks 

veera