Hi,
Im am using DM6435 with Aptina MT9V024 cmos color sensor. I am using debayer interpolation inside prview engine. I obtain colours with too much red, and I have doubt about color of first pixel. At page 96 of spru977A is reported that the first input pixel should be a red pixel. I think that it is specified by initial position defined by SPH and SLV parameters of HORZ_INFO and VERT_START preview registers.
My sensor has this pattern
B Gb B Gb B Gb B........
Gr R Gr R Gr R Gr.......
B Gb B Gb B Gb B........
and so on.
By spru977a SPH must be >= 2, then if I want select first red pixel, I must use SPH = 3 and SLV = 1 ( if SLV = 0 is the first line and EPH = 0 is the first column.....)
I would understand if I think correct, or better how use theese parameters.
Please, can anyone help me?
Thanks
Fabrizio