DM355 EVM has VDD_VIN on the micro connected to 3.3V. According to the datasheet, voltage range for VDD_VIN is 3.135V to 3.465V. However, the EVM has a provision to connect VDD_VIN of the micro to 1.8V. Can I connect VDD_VIN to 1.8V? I have an image sensor that has I/O at 1.8V.