A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts,
I am in planing of an absolutly minimalistic microserver using the OMAP L138 with one SATA Drive and Network plus USB-OTG. Thats all.
However, the OS (EmDebian) should be on a NAND Flash and I neeed a huge amount of DDR2 memory and In the datasheet I see, I can use up to 512MByte DDR2 Memory
OK, I have following availabel:
Micron MT29F4G08AAA (NAND, 4Gbit, 512M x 8)
Micron MT47H128M16 (DDR2, 16M x 16 x 8 banks)
Can I use it for the L138?
Thanks in Advance
Michelle